<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックNo Flash Operation After Power-Up</title>
    <link>https://community.nxp.com/t5/S32K/No-Flash-Operation-After-Power-Up/m-p/1569172#M19418</link>
    <description>&lt;P&gt;I am using a PEmicro Multilink to develop and flash code into my target board with IAR Embedded Workbench.&amp;nbsp; This works fine when the debugger is connected, and I get a UART prompt and some flashing LEDs (to let me know the firmware is running).&lt;/P&gt;&lt;P&gt;If I remove the debugger and cycle power the code does not appear to work: no UART prompt and no flashing LEDs.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When flashing I get the warning below, so I assume that I've got something improperly set in either my linker command file or project settings.&amp;nbsp; Most of the code I'm using, at least for start-up, is from NXP's RTD (version 4.4.2.0.0) for the processor I'm using.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Andy_B_0-1670965285117.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/204256i0E7BF404B07C67E7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Andy_B_0-1670965285117.png" alt="Andy_B_0-1670965285117.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Any insight into how to resolve this would be appreciated.&amp;nbsp; Thank you in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 13 Dec 2022 21:05:06 GMT</pubDate>
    <dc:creator>Andy_B</dc:creator>
    <dc:date>2022-12-13T21:05:06Z</dc:date>
    <item>
      <title>No Flash Operation After Power-Up</title>
      <link>https://community.nxp.com/t5/S32K/No-Flash-Operation-After-Power-Up/m-p/1569172#M19418</link>
      <description>&lt;P&gt;I am using a PEmicro Multilink to develop and flash code into my target board with IAR Embedded Workbench.&amp;nbsp; This works fine when the debugger is connected, and I get a UART prompt and some flashing LEDs (to let me know the firmware is running).&lt;/P&gt;&lt;P&gt;If I remove the debugger and cycle power the code does not appear to work: no UART prompt and no flashing LEDs.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When flashing I get the warning below, so I assume that I've got something improperly set in either my linker command file or project settings.&amp;nbsp; Most of the code I'm using, at least for start-up, is from NXP's RTD (version 4.4.2.0.0) for the processor I'm using.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Andy_B_0-1670965285117.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/204256i0E7BF404B07C67E7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Andy_B_0-1670965285117.png" alt="Andy_B_0-1670965285117.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Any insight into how to resolve this would be appreciated.&amp;nbsp; Thank you in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Dec 2022 21:05:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/No-Flash-Operation-After-Power-Up/m-p/1569172#M19418</guid>
      <dc:creator>Andy_B</dc:creator>
      <dc:date>2022-12-13T21:05:06Z</dc:date>
    </item>
    <item>
      <title>Re: No Flash Operation After Power-Up</title>
      <link>https://community.nxp.com/t5/S32K/No-Flash-Operation-After-Power-Up/m-p/1569331#M19422</link>
      <description>&lt;P&gt;Hi&amp;nbsp;Andy_B,&lt;/P&gt;
&lt;P&gt;Looks more related to IAR, please contact IAR's technical support. I'm not familiar with the use of IAR, but maybe you can refer to this: &lt;A href="https://www.iar.com/knowledge/support/technical-notes/general/creating-a-bootloader-for-cortex-m/" target="_blank"&gt;https://www.iar.com/knowledge/support/technical-notes/general/creating-a-bootloader-for-cortex-m/&lt;/A&gt;&lt;BR /&gt;Also, have you tried the 'Attach to Running Target' feature to see where the program goes wrong?&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 14 Dec 2022 03:32:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/No-Flash-Operation-After-Power-Up/m-p/1569331#M19422</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-12-14T03:32:02Z</dc:date>
    </item>
  </channel>
</rss>