<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K144 EEPROM partition error in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-EEPROM-partition-error/m-p/1565613#M19286</link>
    <description>&lt;P&gt;When I use JLINK to execute, the chip locks and prompts "Device is secure, Erase to unsecure?"Does that mean the chip will not work?Can I solve it?&lt;/P&gt;</description>
    <pubDate>Wed, 07 Dec 2022 05:37:41 GMT</pubDate>
    <dc:creator>lengrudie</dc:creator>
    <dc:date>2022-12-07T05:37:41Z</dc:date>
    <item>
      <title>S32K144 EEPROM partition error</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-EEPROM-partition-error/m-p/1564818#M19241</link>
      <description>&lt;H1&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;I use S32K144-Q100 .&lt;/FONT&gt;&lt;/H1&gt;&lt;P&gt;By default, the FlexNVM partition of the chip is 4 (that is, 64k E-Flash), but I want to change it to partition code 3 (that is, 32k E-Flash), but after using the 0x80 command, an ACCERR error is prompted. Please give me a suggestion on how to change the partition code?&lt;/P&gt;&lt;P&gt;Look forward to your reply.&lt;/P&gt;</description>
      <pubDate>Tue, 06 Dec 2022 01:53:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-EEPROM-partition-error/m-p/1564818#M19241</guid>
      <dc:creator>lengrudie</dc:creator>
      <dc:date>2022-12-06T01:53:53Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 EEPROM partition error</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-EEPROM-partition-error/m-p/1565057#M19249</link>
      <description>&lt;P&gt;Hi&amp;nbsp;lengrudie,&lt;/P&gt;
&lt;P&gt;Please read the "3.1.1.1 Program partition command requirements" of &lt;A id="relatedDocsClickPDF_11" class="dtmcustomrulelink" href="https://www.nxp.com/docs/en/application-note/AN11983.pdf" target="_blank" rel="noopener" data-dtmaction="Documentation Section - Results Link Click" data-dtmsubaction="AN11983: Using the S32K1xx EEPROM Functionality – Application Note - NXP - Application Note - English"&gt;&lt;SPAN&gt;AN11983: Using the S32K1xx EEPROM Functionality – Application Note&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="3.1.1.1 Program partition command requirements.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/203194iA08A2659752B60FA/image-size/large?v=v2&amp;amp;px=999" role="button" title="3.1.1.1 Program partition command requirements.png" alt="3.1.1.1 Program partition command requirements.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;3.1.1.1 Program partition command requirements.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 06 Dec 2022 09:06:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-EEPROM-partition-error/m-p/1565057#M19249</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-12-06T09:06:24Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 EEPROM partition error</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-EEPROM-partition-error/m-p/1565483#M19280</link>
      <description>&lt;P&gt;I did not notice this information, thank you! I tried to use the erase instruction 0x44, but this instruction will also prompt an ACCERR error after it is executed. What's the matter? I hope you can give me some advice and look forward to your reply! thank you!&lt;/P&gt;</description>
      <pubDate>Wed, 07 Dec 2022 01:04:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-EEPROM-partition-error/m-p/1565483#M19280</guid>
      <dc:creator>lengrudie</dc:creator>
      <dc:date>2022-12-07T01:04:50Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 EEPROM partition error</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-EEPROM-partition-error/m-p/1565524#M19283</link>
      <description>&lt;P&gt;Partitioning must only be done once. Please &lt;STRONG&gt;mass erase&lt;/STRONG&gt; the MCU.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="3.1 S32K1xx EEE partitioning.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/203277i3CDB26652C8B0825/image-size/large?v=v2&amp;amp;px=999" role="button" title="3.1 S32K1xx EEE partitioning.png" alt="3.1 S32K1xx EEE partitioning.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;3.1 S32K1xx EEE partitioning.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Dec 2022 02:33:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-EEPROM-partition-error/m-p/1565524#M19283</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-12-07T02:33:05Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 EEPROM partition error</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-EEPROM-partition-error/m-p/1565613#M19286</link>
      <description>&lt;P&gt;When I use JLINK to execute, the chip locks and prompts "Device is secure, Erase to unsecure?"Does that mean the chip will not work?Can I solve it?&lt;/P&gt;</description>
      <pubDate>Wed, 07 Dec 2022 05:37:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-EEPROM-partition-error/m-p/1565613#M19286</guid>
      <dc:creator>lengrudie</dc:creator>
      <dc:date>2022-12-07T05:37:41Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 EEPROM partition error</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-EEPROM-partition-error/m-p/1565623#M19287</link>
      <description>&lt;P&gt;How did you mass erase? SEGGER J-Link Commander and J-Flash is able to mass erase. Click &lt;STRONG&gt;Yes&lt;/STRONG&gt; when&amp;nbsp;&lt;SPAN&gt;prompts&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;"&lt;EM&gt;Device is secure, Erase to unsecure&lt;/EM&gt;?" should also trigger mass erase. After mass erase, you should able to program the chip again. If not, please check the values of MDM-AP status and control registers by refer to:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/Unbricking-S32K146/m-p/937227" target="_self"&gt;Unbricking S32K146&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Dec 2022 05:47:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-EEPROM-partition-error/m-p/1565623#M19287</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-12-07T05:47:32Z</dc:date>
    </item>
  </channel>
</rss>