<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Microcontroller virtualization support for HW seperation</title>
    <link>https://community.nxp.com/t5/S32K/Microcontroller-virtualization-support-for-HW-seperation/m-p/1565416#M19275</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Given that the S32Z is not publicly released, we do recommend to review this directly with your local NXP representative (if you have any).&lt;/P&gt;&lt;P&gt;As to my thoughts, the module should be similar (if not the same) as the ones present in the S32K and S32G.&lt;/P&gt;&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
    <pubDate>Tue, 06 Dec 2022 20:08:51 GMT</pubDate>
    <dc:creator>Daniel-Aguirre</dc:creator>
    <dc:date>2022-12-06T20:08:51Z</dc:date>
    <item>
      <title>Microcontroller virtualization support for HW seperation</title>
      <link>https://community.nxp.com/t5/S32K/Microcontroller-virtualization-support-for-HW-seperation/m-p/1565194#M19261</link>
      <description>&lt;P&gt;Hello NxP Experts, Is there any microcontroller which supports physical HW separation for zone domains? If yes, is it standard virtualization HW support or specific to NxP ? Who are all the hypervisor vendors ?&lt;/P&gt;</description>
      <pubDate>Tue, 06 Dec 2022 13:00:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Microcontroller-virtualization-support-for-HW-seperation/m-p/1565194#M19261</guid>
      <dc:creator>BalrajRamalingam</dc:creator>
      <dc:date>2022-12-06T13:00:08Z</dc:date>
    </item>
    <item>
      <title>Re: Microcontroller virtualization support for HW seperation</title>
      <link>https://community.nxp.com/t5/S32K/Microcontroller-virtualization-support-for-HW-seperation/m-p/1565358#M19272</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Currently, S32x family has an integrated "XRDC" module which helps with the implementation of "domains" inside the same platform. The following is said:&lt;/P&gt;
&lt;P&gt;"A domain typically consists of one or more master, along with the memories and peripherals those masters are allowed to access. &lt;BR /&gt;Because it is access-controlled, a domain acts as an independent computing environment." [Page 529, S32K3xx Reference Manual, Rev. 5, 09/2022].&lt;/P&gt;
&lt;P&gt;The above was extracted from the S32K3 RM, but the same is true for the S32G platform.&lt;/P&gt;
&lt;P&gt;Please, let us know if this information was helpful or not.&lt;/P&gt;</description>
      <pubDate>Tue, 06 Dec 2022 18:16:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Microcontroller-virtualization-support-for-HW-seperation/m-p/1565358#M19272</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2022-12-06T18:16:29Z</dc:date>
    </item>
    <item>
      <title>Re: Microcontroller virtualization support for HW seperation</title>
      <link>https://community.nxp.com/t5/S32K/Microcontroller-virtualization-support-for-HW-seperation/m-p/1565362#M19274</link>
      <description>Hi Daniel,&lt;BR /&gt;That's very clear, on following this, What's virtualization support in S32Z zonal controller? Is it same XRDC or any other Virtualization extension unit is there ? I gone through some slides of S32Z into, they say HW supported virtualization support . Could you please describe what's difference between HW supported hypervisor support means ? My assumption is that there's a special HW support in S32Z for domain isolation.</description>
      <pubDate>Tue, 06 Dec 2022 18:21:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Microcontroller-virtualization-support-for-HW-seperation/m-p/1565362#M19274</guid>
      <dc:creator>BalrajRamalingam</dc:creator>
      <dc:date>2022-12-06T18:21:19Z</dc:date>
    </item>
    <item>
      <title>Re: Microcontroller virtualization support for HW seperation</title>
      <link>https://community.nxp.com/t5/S32K/Microcontroller-virtualization-support-for-HW-seperation/m-p/1565416#M19275</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Given that the S32Z is not publicly released, we do recommend to review this directly with your local NXP representative (if you have any).&lt;/P&gt;&lt;P&gt;As to my thoughts, the module should be similar (if not the same) as the ones present in the S32K and S32G.&lt;/P&gt;&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Tue, 06 Dec 2022 20:08:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Microcontroller-virtualization-support-for-HW-seperation/m-p/1565416#M19275</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2022-12-06T20:08:51Z</dc:date>
    </item>
  </channel>
</rss>