<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Error Correcting Code (ECC) in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Error-Correcting-Code-ECC/m-p/1561539#M19134</link>
    <description>&lt;P&gt;Hello All.&lt;/P&gt;&lt;P&gt;I am Working On Some Project on [ S32k312 MCU]&amp;nbsp;Using:&lt;BR /&gt;Compiler ==&amp;gt; GHS MultiTool&amp;nbsp;&lt;BR /&gt;Debugger ==&amp;gt; Lauterbach Trace 32&amp;nbsp;&lt;/P&gt;&lt;P&gt;MCAL Integrator Tool ==&amp;gt; EB Tressos Studio&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;The problem is when I Inject Multi Bit Errors using EIM Module to the SRAM0&amp;nbsp;&lt;BR /&gt;The MCU Raises A bus Fault Exception&amp;nbsp;&lt;BR /&gt;While I Followed The Steps in Reference Manual.&lt;/P&gt;&lt;P&gt;I was Waiting to see the ERM Multibit Error ISR To be called but this is not the Case.&lt;BR /&gt;&lt;BR /&gt;I Searched About the problem and Found That XRDC May be restricting access to this RAM Location and may be the reason this fault happens&amp;nbsp;&lt;/P&gt;&lt;P&gt;but&amp;nbsp;later I found that the XRDC is not Configured From Tressos Studio.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;So Two Questions are there ?&amp;nbsp;&lt;BR /&gt;1) What could be the Reasons to this bus Fault ?&lt;BR /&gt;2)How To know Configure XRDC Module in Tressos Studio ?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thanks A lot&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 29 Nov 2022 20:48:22 GMT</pubDate>
    <dc:creator>MohamedSalah</dc:creator>
    <dc:date>2022-11-29T20:48:22Z</dc:date>
    <item>
      <title>Error Correcting Code (ECC)</title>
      <link>https://community.nxp.com/t5/S32K/Error-Correcting-Code-ECC/m-p/1561539#M19134</link>
      <description>&lt;P&gt;Hello All.&lt;/P&gt;&lt;P&gt;I am Working On Some Project on [ S32k312 MCU]&amp;nbsp;Using:&lt;BR /&gt;Compiler ==&amp;gt; GHS MultiTool&amp;nbsp;&lt;BR /&gt;Debugger ==&amp;gt; Lauterbach Trace 32&amp;nbsp;&lt;/P&gt;&lt;P&gt;MCAL Integrator Tool ==&amp;gt; EB Tressos Studio&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;The problem is when I Inject Multi Bit Errors using EIM Module to the SRAM0&amp;nbsp;&lt;BR /&gt;The MCU Raises A bus Fault Exception&amp;nbsp;&lt;BR /&gt;While I Followed The Steps in Reference Manual.&lt;/P&gt;&lt;P&gt;I was Waiting to see the ERM Multibit Error ISR To be called but this is not the Case.&lt;BR /&gt;&lt;BR /&gt;I Searched About the problem and Found That XRDC May be restricting access to this RAM Location and may be the reason this fault happens&amp;nbsp;&lt;/P&gt;&lt;P&gt;but&amp;nbsp;later I found that the XRDC is not Configured From Tressos Studio.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;So Two Questions are there ?&amp;nbsp;&lt;BR /&gt;1) What could be the Reasons to this bus Fault ?&lt;BR /&gt;2)How To know Configure XRDC Module in Tressos Studio ?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thanks A lot&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Nov 2022 20:48:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Error-Correcting-Code-ECC/m-p/1561539#M19134</guid>
      <dc:creator>MohamedSalah</dc:creator>
      <dc:date>2022-11-29T20:48:22Z</dc:date>
    </item>
    <item>
      <title>Re: Error Correcting Code (ECC)</title>
      <link>https://community.nxp.com/t5/S32K/Error-Correcting-Code-ECC/m-p/1566833#M19334</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;MohamedSalah,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;1. The Bus fault occurred because had a write command to the memory area where EIM was injected error complete.&lt;/P&gt;
&lt;P&gt;In some situations, the debugger can cause the bus fault error. So, you can test with turn off the debugger and using blink-led statements to inform the test is successful.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;2. To configure&amp;nbsp;XRDC, you can refer to the&amp;nbsp;RTD_RM_UM.pdf file in the RM module in the package.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Dan&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 08 Dec 2022 11:36:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Error-Correcting-Code-ECC/m-p/1566833#M19334</guid>
      <dc:creator>DanNguyenDuy</dc:creator>
      <dc:date>2022-12-08T11:36:23Z</dc:date>
    </item>
    <item>
      <title>Re: Error Correcting Code (ECC)</title>
      <link>https://community.nxp.com/t5/S32K/Error-Correcting-Code-ECC/m-p/1568650#M19398</link>
      <description>&lt;P&gt;Thanks Dan for your reply&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Dec 2022 00:37:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Error-Correcting-Code-ECC/m-p/1568650#M19398</guid>
      <dc:creator>MohamedSalah</dc:creator>
      <dc:date>2022-12-13T00:37:06Z</dc:date>
    </item>
  </channel>
</rss>