<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CSEC S32K1 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/CSEC-S32K1/m-p/1560468#M19108</link>
    <description>&lt;P&gt;I want to ask how do I determine whether the key of CSEC is encrypted when I use CSEC, because I cannot perform factory settings, and how do I determine whether the key is encrypted?thanks&lt;/P&gt;</description>
    <pubDate>Mon, 28 Nov 2022 09:01:44 GMT</pubDate>
    <dc:creator>QJ_HAPPY</dc:creator>
    <dc:date>2022-11-28T09:01:44Z</dc:date>
    <item>
      <title>CSEC S32K1</title>
      <link>https://community.nxp.com/t5/S32K/CSEC-S32K1/m-p/1560468#M19108</link>
      <description>&lt;P&gt;I want to ask how do I determine whether the key of CSEC is encrypted when I use CSEC, because I cannot perform factory settings, and how do I determine whether the key is encrypted?thanks&lt;/P&gt;</description>
      <pubDate>Mon, 28 Nov 2022 09:01:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CSEC-S32K1/m-p/1560468#M19108</guid>
      <dc:creator>QJ_HAPPY</dc:creator>
      <dc:date>2022-11-28T09:01:44Z</dc:date>
    </item>
    <item>
      <title>Re: CSEC S32K1</title>
      <link>https://community.nxp.com/t5/S32K/CSEC-S32K1/m-p/1561584#M19137</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/197531"&gt;@QJ_HAPPY&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Each key has 6 flag associated with it, one of these is Key Usage Flag (KEY_USAGE), that determines if a key is used for encryption/decryption or for CMAC generation/verification.&lt;BR /&gt;Regarding of how to return to the factory settings when CSE is enabled, the only way to restore it is with a mass erase, for this you need to run CMD_DBG_CHAL and CMD_DBG_AUTH commands to destroy the partition and then you can run mass erase. But if any CSEc key is ‘write-protected’ the above procedure will not work thus mass erase cannot be launched.&lt;/P&gt;
&lt;P&gt;Take a look to these application notes, they will be useful for you.&lt;BR /&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN5401" target="_blank" rel="noopener"&gt;Getting Started with CSEc Security Module&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12130.pdf?_gl=1*1b60mfs*_ga*MTMwNjI3NjYxOC4xNjY5NzU4NjQ0*_ga_WM5LE0KMSH*MTY2OTc1ODY0My4xLjEuMTY2OTc2MjA0Ni4wLjAuMA.." target="_self"&gt;Production Flash Programming Best Practices for S32K1xx MCUs&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Tue, 29 Nov 2022 23:42:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CSEC-S32K1/m-p/1561584#M19137</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2022-11-29T23:42:52Z</dc:date>
    </item>
  </channel>
</rss>