<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K144 CAN command lost in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-CAN-command-lost/m-p/1560290#M19101</link>
    <description>&lt;P&gt;When the amount of CAN communication data is large,some CAN commands are lost becasue the commands can't be processed in time in S32K144. What are some ways to solve it?Are there any specific instructions?&lt;/P&gt;</description>
    <pubDate>Mon, 28 Nov 2022 04:20:44 GMT</pubDate>
    <dc:creator>jingfang</dc:creator>
    <dc:date>2022-11-28T04:20:44Z</dc:date>
    <item>
      <title>S32K144 CAN command lost</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-CAN-command-lost/m-p/1560290#M19101</link>
      <description>&lt;P&gt;When the amount of CAN communication data is large,some CAN commands are lost becasue the commands can't be processed in time in S32K144. What are some ways to solve it?Are there any specific instructions?&lt;/P&gt;</description>
      <pubDate>Mon, 28 Nov 2022 04:20:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-CAN-command-lost/m-p/1560290#M19101</guid>
      <dc:creator>jingfang</dc:creator>
      <dc:date>2022-11-28T04:20:44Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 CAN command lost</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-CAN-command-lost/m-p/1561530#M19133</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;if CPU needs more time to serve MBs you can implement a so called reception queue as mentioned in Matching chapter of the RM&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PetrS_0-1669752383571.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/202156i0C91C7B1B4BFB7DF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="PetrS_0-1669752383571.png" alt="PetrS_0-1669752383571.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;PetrS_0-1669752383571.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Or enable and use RXFIFO which can hold up to 6 messages and also the DMA can be used to read messages out of RXFIFO. Note&amp;nbsp;Rx FIFO must not be enabled when CAN FD feature is&lt;BR /&gt;enabled.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Tue, 29 Nov 2022 20:09:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-CAN-command-lost/m-p/1561530#M19133</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-11-29T20:09:19Z</dc:date>
    </item>
  </channel>
</rss>