<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K144   LPUART1_RxTx_IRQHandler in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-LPUART1-RxTx-IRQHandler/m-p/736024#M1885</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, it can be done this way.&lt;/P&gt;&lt;P&gt;See attached LPUART demo example with added RX interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Nov 2017 13:18:09 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2017-11-02T13:18:09Z</dc:date>
    <item>
      <title>S32K144   LPUART1_RxTx_IRQHandler</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-LPUART1-RxTx-IRQHandler/m-p/736023#M1884</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to enable the computer to send the data to the S32 MCU, and then print it to the computer terminal. I don't know if I have the correct writing below, I would like to give directions.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11703i351377DF55D9E092/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Oct 2017 09:53:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-LPUART1-RxTx-IRQHandler/m-p/736023#M1884</guid>
      <dc:creator>wangfei11</dc:creator>
      <dc:date>2017-10-31T09:53:00Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144   LPUART1_RxTx_IRQHandler</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-LPUART1-RxTx-IRQHandler/m-p/736024#M1885</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, it can be done this way.&lt;/P&gt;&lt;P&gt;See attached LPUART demo example with added RX interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Nov 2017 13:18:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-LPUART1-RxTx-IRQHandler/m-p/736024#M1885</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-11-02T13:18:09Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144   LPUART1_RxTx_IRQHandler</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-LPUART1-RxTx-IRQHandler/m-p/736025#M1886</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was trying to do the same thing Receiving an RX interrupt but I can't make it work, I am able to send data through TX, interrupts just for RX and baudrate 115200. can you help if I am missing something please. I am using S32K146&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I already enabled the Transmitter and Receiver and enable Receiver Interrupt.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Dec 2019 19:35:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-LPUART1-RxTx-IRQHandler/m-p/736025#M1886</guid>
      <dc:creator>tonymor90</dc:creator>
      <dc:date>2019-12-17T19:35:49Z</dc:date>
    </item>
  </channel>
</rss>