<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K144 with LCD 1602A in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-with-LCD-1602A/m-p/1553024#M18845</link>
    <description>&lt;P&gt;Hi&amp;nbsp;gksn284,&lt;/P&gt;
&lt;P&gt;I didn't find any ready code for s32k144 to implement LCD 1602A. However, you can refer to the following post using Kinetis MCU:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Driving-16x2-LCD-using-KSDK-drivers/ta-p/1098903" target="_self"&gt;&lt;SPAN class="lia-link-navigation lia-link-disabled"&gt;Driving 16x2 LCD using KSDK drivers&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Mon, 14 Nov 2022 06:56:14 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2022-11-14T06:56:14Z</dc:date>
    <item>
      <title>S32K144 with LCD 1602A</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-with-LCD-1602A/m-p/1552841#M18839</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I want to use LCD in S32K144. (&lt;/SPAN&gt;LCD 1602A or LCD 1602A + I2C)&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is there no related library or code?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please help me.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 13 Nov 2022 14:13:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-with-LCD-1602A/m-p/1552841#M18839</guid>
      <dc:creator>gksn284</dc:creator>
      <dc:date>2022-11-13T14:13:49Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 with LCD 1602A</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-with-LCD-1602A/m-p/1553024#M18845</link>
      <description>&lt;P&gt;Hi&amp;nbsp;gksn284,&lt;/P&gt;
&lt;P&gt;I didn't find any ready code for s32k144 to implement LCD 1602A. However, you can refer to the following post using Kinetis MCU:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Driving-16x2-LCD-using-KSDK-drivers/ta-p/1098903" target="_self"&gt;&lt;SPAN class="lia-link-navigation lia-link-disabled"&gt;Driving 16x2 LCD using KSDK drivers&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 14 Nov 2022 06:56:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-with-LCD-1602A/m-p/1553024#M18845</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-11-14T06:56:14Z</dc:date>
    </item>
  </channel>
</rss>