<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K144 ADC_HW Triggering error</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-ADC-HW-Triggering-error/m-p/1552609#M18831</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;from the code I do not see calibration is started for ADC1. Also do not do it parallelly. Calibrate ADCs modules in sequence.&lt;BR /&gt;See steps to do in chapter&amp;nbsp;44.5.6 Calibration function of the RM.&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 11 Nov 2022 12:06:48 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2022-11-11T12:06:48Z</dc:date>
    <item>
      <title>S32K144 ADC_HW Triggering error</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-ADC-HW-Triggering-error/m-p/1551042#M18775</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;i wanted to use 10xADC channels. I used 7xADC0 and 3xADC1 for my application. Initially i started with 7xADC0 using PDB triggering with interrupt and it was working. Now i want to add 3xADC1 using PDB, so that there is a total of 10 ADC. Unfortunately, my code does not work for the same and gets stuck in the calibration part. Attached the code below&lt;/P&gt;</description>
      <pubDate>Wed, 09 Nov 2022 12:03:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-ADC-HW-Triggering-error/m-p/1551042#M18775</guid>
      <dc:creator>Adhi_11</dc:creator>
      <dc:date>2022-11-09T12:03:21Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 ADC_HW Triggering error</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-ADC-HW-Triggering-error/m-p/1552609#M18831</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;from the code I do not see calibration is started for ADC1. Also do not do it parallelly. Calibrate ADCs modules in sequence.&lt;BR /&gt;See steps to do in chapter&amp;nbsp;44.5.6 Calibration function of the RM.&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Nov 2022 12:06:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-ADC-HW-Triggering-error/m-p/1552609#M18831</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-11-11T12:06:48Z</dc:date>
    </item>
  </channel>
</rss>