<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Why S32K3 do not add UART IDLE function? in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Why-S32K3-do-not-add-UART-IDLE-function/m-p/1549676#M18710</link>
    <description>&lt;P&gt;&lt;FONT&gt;Hi Xianlong,&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT&gt;the drivers usually do not cover 100% functionality of the device and this is the case of idle detection. There was no such requirement to support this feature in the drivers. &lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT&gt;There are no issues with this feature. I'm afraid that currently the only option is to implement the functionality by yourself. &lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT&gt;Regards,&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT&gt;Lukas&lt;/FONT&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 07 Nov 2022 12:20:47 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2022-11-07T12:20:47Z</dc:date>
    <item>
      <title>Why S32K3 do not add UART IDLE function?</title>
      <link>https://community.nxp.com/t5/S32K/Why-S32K3-do-not-add-UART-IDLE-function/m-p/1549380#M18701</link>
      <description>&lt;P&gt;Hi,All&lt;/P&gt;&lt;P&gt;I use UART IDLE&amp;nbsp; to implement "UART receive indefinite length data".&lt;BR /&gt;But RTD2.0.0 don't have the idle function API,I need to change the code.&lt;BR /&gt;&lt;FONT&gt;I wonder why S32K3_RTD does not implement idle function, is there any hidden danger? I find this feature very useful.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;xianlong&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 07 Nov 2022 06:04:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Why-S32K3-do-not-add-UART-IDLE-function/m-p/1549380#M18701</guid>
      <dc:creator>xianlong</dc:creator>
      <dc:date>2022-11-07T06:04:25Z</dc:date>
    </item>
    <item>
      <title>Re: Why S32K3 do not add UART IDLE function?</title>
      <link>https://community.nxp.com/t5/S32K/Why-S32K3-do-not-add-UART-IDLE-function/m-p/1549676#M18710</link>
      <description>&lt;P&gt;&lt;FONT&gt;Hi Xianlong,&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT&gt;the drivers usually do not cover 100% functionality of the device and this is the case of idle detection. There was no such requirement to support this feature in the drivers. &lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT&gt;There are no issues with this feature. I'm afraid that currently the only option is to implement the functionality by yourself. &lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT&gt;Regards,&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT&gt;Lukas&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 07 Nov 2022 12:20:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Why-S32K3-do-not-add-UART-IDLE-function/m-p/1549676#M18710</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-11-07T12:20:47Z</dc:date>
    </item>
  </channel>
</rss>