<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32144-CAN_SRXDIS in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32144-CAN-SRXDIS/m-p/1543914#M18540</link>
    <description>yes, your are right !&lt;BR /&gt;Thank you very much !</description>
    <pubDate>Wed, 26 Oct 2022 08:26:27 GMT</pubDate>
    <dc:creator>Junkie</dc:creator>
    <dc:date>2022-10-26T08:26:27Z</dc:date>
    <item>
      <title>S32144-CAN_SRXDIS</title>
      <link>https://community.nxp.com/t5/S32K/S32144-CAN-SRXDIS/m-p/1541938#M18477</link>
      <description>&lt;P&gt;I try to use FlexCAN MB0 to receive CAN frames transmitted&amp;nbsp; by itself-MB1, just like describled in RM "when MCR[SRXDIS] is deasserted,&amp;nbsp;FlexCAN can receive frames transmitted by itself if a matching Rx mailbox exists. "&lt;/P&gt;&lt;P&gt;i initlization CAN0 normally and corrsponding pin, and clear MCR_SRXDIS, configure MB0 with ID 0x3AA, MB_CS_CODE = EMPTY, and then configure MB1 with ID 0x3AA, data0~8 bytes, MB_CS_CODE = DATA.But it does not work, PTB1 does not stop transmit frames, but FlexCAN can not received.&lt;/P&gt;&lt;P&gt;(CAN transceiver is connected)&lt;/P&gt;</description>
      <pubDate>Fri, 21 Oct 2022 10:32:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32144-CAN-SRXDIS/m-p/1541938#M18477</guid>
      <dc:creator>Junkie</dc:creator>
      <dc:date>2022-10-21T10:32:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32144-CAN_SRXDIS</title>
      <link>https://community.nxp.com/t5/S32K/S32144-CAN-SRXDIS/m-p/1541992#M18481</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;be sure SRXDIS is really cleared, can be written in Freeze mode only.&lt;BR /&gt;Also note that only successfully transmitted message without error will be self-received. So for example if other node does not ACK a message it is repeated still and it is not received. Which is probably you have.&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 21 Oct 2022 13:19:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32144-CAN-SRXDIS/m-p/1541992#M18481</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-10-21T13:19:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32144-CAN_SRXDIS</title>
      <link>https://community.nxp.com/t5/S32K/S32144-CAN-SRXDIS/m-p/1543914#M18540</link>
      <description>yes, your are right !&lt;BR /&gt;Thank you very much !</description>
      <pubDate>Wed, 26 Oct 2022 08:26:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32144-CAN-SRXDIS/m-p/1543914#M18540</guid>
      <dc:creator>Junkie</dc:creator>
      <dc:date>2022-10-26T08:26:27Z</dc:date>
    </item>
  </channel>
</rss>