<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: Request S32K3 MCAL FlexCAN Example</title>
    <link>https://community.nxp.com/t5/S32K/Request-S32K3-MCAL-FlexCAN-Example/m-p/1537877#M18326</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;could below example be helpful?&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225&lt;/A&gt;&lt;BR /&gt;But it is using FlexCAN IP driver.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Fri, 14 Oct 2022 13:12:14 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2022-10-14T13:12:14Z</dc:date>
    <item>
      <title>Request S32K3 MCAL FlexCAN Example</title>
      <link>https://community.nxp.com/t5/S32K/Request-S32K3-MCAL-FlexCAN-Example/m-p/1536690#M18271</link>
      <description>&lt;P&gt;Do you have a FlexCAN example made by MCAL driver on S32K344-EVB ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm developing a FlexCAN example on S32K3X4EVB-Q257 board. The example code is made by MCAL driver. But that example (CAN_example_CT.mex) is work on Loopback mode and Polling operation. I did modify that example to not Loopback using CAN0 pins.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I verified basic operation using CAN API (Can_MainFunction_Write, Can_MainFunction_Read).&lt;/P&gt;&lt;P&gt;But the configuration of FlexCAN is works on one kind of Message ID. When config is Standard Message ID the Extended ID can't works. When config is Extended ID the Standard ID can't works.&lt;/P&gt;&lt;P&gt;I confuse relation between Message ID and Message Buffer (MailBox). For more Message ID and StandardFifo, LegacyFifo and ExtendedFio.&lt;/P&gt;&lt;P&gt;Could you tell me how to works Standard ID and Extended ID ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My development is base on following.&lt;/P&gt;&lt;P&gt;- S32DS 3.4&lt;/P&gt;&lt;P&gt;- SDK is&amp;nbsp;PlatformSDK_S32K3_2022_07&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 13 Oct 2022 02:00:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Request-S32K3-MCAL-FlexCAN-Example/m-p/1536690#M18271</guid>
      <dc:creator>dnewbe</dc:creator>
      <dc:date>2022-10-13T02:00:43Z</dc:date>
    </item>
    <item>
      <title>Re: Request S32K3 MCAL FlexCAN Example</title>
      <link>https://community.nxp.com/t5/S32K/Request-S32K3-MCAL-FlexCAN-Example/m-p/1537877#M18326</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;could below example be helpful?&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225&lt;/A&gt;&lt;BR /&gt;But it is using FlexCAN IP driver.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Fri, 14 Oct 2022 13:12:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Request-S32K3-MCAL-FlexCAN-Example/m-p/1537877#M18326</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-10-14T13:12:14Z</dc:date>
    </item>
    <item>
      <title>Re: Request S32K3 MCAL FlexCAN Example</title>
      <link>https://community.nxp.com/t5/S32K/Request-S32K3-MCAL-FlexCAN-Example/m-p/1540612#M18427</link>
      <description>&lt;P&gt;Thanks PetrS&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But I need MCAL driver because I did make other driver is make with MCAL driver like as LIN and PIT etc.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 20 Oct 2022 01:16:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Request-S32K3-MCAL-FlexCAN-Example/m-p/1540612#M18427</guid>
      <dc:creator>dnewbe</dc:creator>
      <dc:date>2022-10-20T01:16:16Z</dc:date>
    </item>
    <item>
      <title>Re: Request S32K3 MCAL FlexCAN Example</title>
      <link>https://community.nxp.com/t5/S32K/Request-S32K3-MCAL-FlexCAN-Example/m-p/1541188#M18446</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;try this...&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K344-EVB-With-MCAL-FLEXCAN-TJA1153/td-p/1540687" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K344-EVB-With-MCAL-FLEXCAN-TJA1153/td-p/1540687&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 20 Oct 2022 13:17:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Request-S32K3-MCAL-FlexCAN-Example/m-p/1541188#M18446</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-10-20T13:17:41Z</dc:date>
    </item>
  </channel>
</rss>