<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックEthernet PHY Over SPI Example</title>
    <link>https://community.nxp.com/t5/S32K/Ethernet-PHY-Over-SPI-Example/m-p/1536695#M18273</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working on integrating an Ethernet PHY that uses SPI as its interface with the MCU. I see the example projects that utilize Eth module in Tresos are using MII interfaces instead. Are there any support material that might help shed some light on using SPI as its interface?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Thu, 13 Oct 2022 02:09:26 GMT</pubDate>
    <dc:creator>Engietoday</dc:creator>
    <dc:date>2022-10-13T02:09:26Z</dc:date>
    <item>
      <title>Ethernet PHY Over SPI Example</title>
      <link>https://community.nxp.com/t5/S32K/Ethernet-PHY-Over-SPI-Example/m-p/1536695#M18273</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working on integrating an Ethernet PHY that uses SPI as its interface with the MCU. I see the example projects that utilize Eth module in Tresos are using MII interfaces instead. Are there any support material that might help shed some light on using SPI as its interface?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 13 Oct 2022 02:09:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Ethernet-PHY-Over-SPI-Example/m-p/1536695#M18273</guid>
      <dc:creator>Engietoday</dc:creator>
      <dc:date>2022-10-13T02:09:26Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet PHY Over SPI Example</title>
      <link>https://community.nxp.com/t5/S32K/Ethernet-PHY-Over-SPI-Example/m-p/1537801#M18322</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;as we do not offer Ethernet PHY with SPI interface then we will have no example for that. Moreover I do not know such devices, maybe Ethernet controller (MAC+PHY) with SPI. Anyway for SPI examples refer to SPI demos in Tresos or S32DS.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Fri, 14 Oct 2022 10:41:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Ethernet-PHY-Over-SPI-Example/m-p/1537801#M18322</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-10-14T10:41:34Z</dc:date>
    </item>
  </channel>
</rss>