<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックopenSDA USB connection</title>
    <link>https://community.nxp.com/t5/S32K/openSDA-USB-connection/m-p/1536200#M18259</link>
    <description>&lt;P&gt;Hello everyone,&lt;BR /&gt;&lt;BR /&gt;I am back with some other doubts. Kindly take out some time to help me out.&lt;BR /&gt;&lt;BR /&gt;I am attaching the screenshot of the opensda schematic input via USB. I have the following doubts:&lt;BR /&gt;1. What are these L1 and L2? I believe these are inductors. If yes, then why is its value in OHMS?&lt;BR /&gt;2. Why are these L1 and L2 used and connected? I understand the use of bypass capacitors along with the power source; but I couldnot figure out the use of these L1 and L2.&lt;BR /&gt;3. Also, kindly help me out in figuring the use of D17, D18 and D19 in the circuit.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ankan_creatara_0-1665569076916.png" style="width: 679px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/196495i849FB1D1A2B07BB7/image-dimensions/679x291?v=v2" width="679" height="291" role="button" title="ankan_creatara_0-1665569076916.png" alt="ankan_creatara_0-1665569076916.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ankan_creatara_0-1665569076916.png&lt;/span&gt;&lt;/span&gt;&lt;BR /&gt;Kindly help me out in understanding the schematic.&lt;BR /&gt;&lt;BR /&gt;Thank you for your time.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 12 Oct 2022 10:07:47 GMT</pubDate>
    <dc:creator>ankan_creatara</dc:creator>
    <dc:date>2022-10-12T10:07:47Z</dc:date>
    <item>
      <title>openSDA USB connection</title>
      <link>https://community.nxp.com/t5/S32K/openSDA-USB-connection/m-p/1536200#M18259</link>
      <description>&lt;P&gt;Hello everyone,&lt;BR /&gt;&lt;BR /&gt;I am back with some other doubts. Kindly take out some time to help me out.&lt;BR /&gt;&lt;BR /&gt;I am attaching the screenshot of the opensda schematic input via USB. I have the following doubts:&lt;BR /&gt;1. What are these L1 and L2? I believe these are inductors. If yes, then why is its value in OHMS?&lt;BR /&gt;2. Why are these L1 and L2 used and connected? I understand the use of bypass capacitors along with the power source; but I couldnot figure out the use of these L1 and L2.&lt;BR /&gt;3. Also, kindly help me out in figuring the use of D17, D18 and D19 in the circuit.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ankan_creatara_0-1665569076916.png" style="width: 679px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/196495i849FB1D1A2B07BB7/image-dimensions/679x291?v=v2" width="679" height="291" role="button" title="ankan_creatara_0-1665569076916.png" alt="ankan_creatara_0-1665569076916.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ankan_creatara_0-1665569076916.png&lt;/span&gt;&lt;/span&gt;&lt;BR /&gt;Kindly help me out in understanding the schematic.&lt;BR /&gt;&lt;BR /&gt;Thank you for your time.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Oct 2022 10:07:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/openSDA-USB-connection/m-p/1536200#M18259</guid>
      <dc:creator>ankan_creatara</dc:creator>
      <dc:date>2022-10-12T10:07:47Z</dc:date>
    </item>
    <item>
      <title>Re: openSDA USB connection</title>
      <link>https://community.nxp.com/t5/S32K/openSDA-USB-connection/m-p/1536259#M18262</link>
      <description>&lt;P&gt;1) L1 and L2 are ferrite beads and 330Ohm is an impedance at 100MHz. If you want to see specific type, for instance following:&lt;BR /&gt;MPZ1608S331A&lt;/P&gt;
&lt;P&gt;2) &lt;A href="https://en.wikipedia.org/wiki/Ferrite_bead" target="_blank" rel="noopener"&gt;https://en.wikipedia.org/wiki/Ferrite_bead&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;3) It is ESD protection diode.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nexperia.com/products/esd-protection-tvs-filtering-and-signal-conditioning/esd-protection/low-capacitance-esd-protection-for-high-speed-interfaces/PESD5V0R1BSF.html" target="_blank" rel="noopener"&gt;https://www.nexperia.com/products/esd-protection-tvs-filtering-and-signal-conditioning/esd-protection/low-capacitance-esd-protection-for-high-speed-interfaces/PESD5V0R1BSF.html&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Oct 2022 12:50:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/openSDA-USB-connection/m-p/1536259#M18262</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2022-10-12T12:50:06Z</dc:date>
    </item>
  </channel>
</rss>