<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Receiving in LPSPI: Cookbook AN5413 vs Reference Manual in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Receiving-in-LPSPI-Cookbook-AN5413-vs-Reference-Manual/m-p/729809#M1816</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the reference manual the LPSPI Status Register (SR) shows the RDF and TDF flags are read-only (see section 46.3.1.5.2). In the AN5413 cookbook the flags&amp;nbsp;are written to 1 to clear them (e.g. in the function LPSPI1_receive_16bits). Is this necessary? Why do the flags&amp;nbsp;need to be written when they are read-only? Is the Application Note correct or is the Reference Manual correct?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Oct 2017 16:46:25 GMT</pubDate>
    <dc:creator>kt1003</dc:creator>
    <dc:date>2017-10-27T16:46:25Z</dc:date>
    <item>
      <title>Receiving in LPSPI: Cookbook AN5413 vs Reference Manual</title>
      <link>https://community.nxp.com/t5/S32K/Receiving-in-LPSPI-Cookbook-AN5413-vs-Reference-Manual/m-p/729809#M1816</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the reference manual the LPSPI Status Register (SR) shows the RDF and TDF flags are read-only (see section 46.3.1.5.2). In the AN5413 cookbook the flags&amp;nbsp;are written to 1 to clear them (e.g. in the function LPSPI1_receive_16bits). Is this necessary? Why do the flags&amp;nbsp;need to be written when they are read-only? Is the Application Note correct or is the Reference Manual correct?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Oct 2017 16:46:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Receiving-in-LPSPI-Cookbook-AN5413-vs-Reference-Manual/m-p/729809#M1816</guid>
      <dc:creator>kt1003</dc:creator>
      <dc:date>2017-10-27T16:46:25Z</dc:date>
    </item>
    <item>
      <title>Re: Receiving in LPSPI: Cookbook AN5413 vs Reference Manual</title>
      <link>https://community.nxp.com/t5/S32K/Receiving-in-LPSPI-Cookbook-AN5413-vs-Reference-Manual/m-p/729810#M1817</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The reference manual is correct.&lt;/P&gt;&lt;P&gt;Tha flags are set/cleared depending on the number of words stored in the FIFOs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Oct 2017 15:27:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Receiving-in-LPSPI-Cookbook-AN5413-vs-Reference-Manual/m-p/729810#M1817</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-10-30T15:27:13Z</dc:date>
    </item>
  </channel>
</rss>