<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Calibrating ADC modules simultaneously on two different cores in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Calibrating-ADC-modules-simultaneously-on-two-different-cores/m-p/1531628#M18091</link>
    <description>&lt;P&gt;&lt;STRONG&gt;Will it be a problem to calibrate two ADC instances simultaneously on two different cores?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The reference manual S32K3XXRM notes that:&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;ADC must be calibrated before it can do meaningful conversions. The application must prevent any start of conversion before&lt;BR /&gt;the ongoing calibration has finished successfully. No conversion trigger may be received during calibration.&lt;/PRE&gt;&lt;P&gt;The calibration is implemented by, among others, powering-down the ADC &lt;STRONG&gt;instance&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;Therefore, it seems to me that one ADC&amp;nbsp;&lt;STRONG&gt;instance&amp;nbsp;&lt;/STRONG&gt;can not do a start of conversion before the ongoing celebration has finished, but another &lt;STRONG&gt;instance&lt;/STRONG&gt; can start a calibration at the same time.&lt;/P&gt;&lt;P&gt;Is my line of thinking correct?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 04 Oct 2022 11:17:41 GMT</pubDate>
    <dc:creator>abemat</dc:creator>
    <dc:date>2022-10-04T11:17:41Z</dc:date>
    <item>
      <title>Calibrating ADC modules simultaneously on two different cores</title>
      <link>https://community.nxp.com/t5/S32K/Calibrating-ADC-modules-simultaneously-on-two-different-cores/m-p/1531628#M18091</link>
      <description>&lt;P&gt;&lt;STRONG&gt;Will it be a problem to calibrate two ADC instances simultaneously on two different cores?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The reference manual S32K3XXRM notes that:&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;ADC must be calibrated before it can do meaningful conversions. The application must prevent any start of conversion before&lt;BR /&gt;the ongoing calibration has finished successfully. No conversion trigger may be received during calibration.&lt;/PRE&gt;&lt;P&gt;The calibration is implemented by, among others, powering-down the ADC &lt;STRONG&gt;instance&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;Therefore, it seems to me that one ADC&amp;nbsp;&lt;STRONG&gt;instance&amp;nbsp;&lt;/STRONG&gt;can not do a start of conversion before the ongoing celebration has finished, but another &lt;STRONG&gt;instance&lt;/STRONG&gt; can start a calibration at the same time.&lt;/P&gt;&lt;P&gt;Is my line of thinking correct?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 04 Oct 2022 11:17:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Calibrating-ADC-modules-simultaneously-on-two-different-cores/m-p/1531628#M18091</guid>
      <dc:creator>abemat</dc:creator>
      <dc:date>2022-10-04T11:17:41Z</dc:date>
    </item>
    <item>
      <title>Re: Calibrating ADC modules simultaneously on two different cores</title>
      <link>https://community.nxp.com/t5/S32K/Calibrating-ADC-modules-simultaneously-on-two-different-cores/m-p/1532549#M18123</link>
      <description>&lt;P&gt;Hi, I don't think it is a good idea, because in such case voltage references could be sampled by two ADCs at once, what's not recommended and should affected conversion accuracy.&lt;/P&gt;
&lt;P&gt;I would recommend to perform ADC calibrations sequentially.&lt;/P&gt;</description>
      <pubDate>Wed, 05 Oct 2022 10:35:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Calibrating-ADC-modules-simultaneously-on-two-different-cores/m-p/1532549#M18123</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2022-10-05T10:35:38Z</dc:date>
    </item>
  </channel>
</rss>