<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K3 AB Swap without HSE</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-AB-Swap-without-HSE/m-p/1529958#M18044</link>
    <description>&lt;P&gt;hi lucas,&lt;/P&gt;&lt;P&gt;Can you tell me that where can i download the SW32K3_OTADEMO_0.8.0_D2203?&lt;/P&gt;&lt;P&gt;thanks a lot.&lt;/P&gt;</description>
    <pubDate>Thu, 29 Sep 2022 02:16:27 GMT</pubDate>
    <dc:creator>PatrickPP</dc:creator>
    <dc:date>2022-09-29T02:16:27Z</dc:date>
    <item>
      <title>S32K3 AB Swap without HSE</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-AB-Swap-without-HSE/m-p/1485321#M16224</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm looking for some clarification regarding the AB Swap functionality. Here the questions:&lt;/P&gt;&lt;P&gt;1. Is it possible to do an AB Swap without the HSE (only sBAF)? Or is HSE required? Is there some demo app for this?&lt;/P&gt;&lt;P&gt;2. Is it possible to change the size of the AB Swap blocks? For example on a S32K312 use only 128 KB (x2 256 KB) and than use the remaining space for other purposes?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Jul 2022 10:43:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-AB-Swap-without-HSE/m-p/1485321#M16224</guid>
      <dc:creator>ValTek</dc:creator>
      <dc:date>2022-07-06T10:43:57Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 AB Swap without HSE</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-AB-Swap-without-HSE/m-p/1485416#M16227</link>
      <description>&lt;P&gt;Hi, probably this is another reply...&lt;/P&gt;</description>
      <pubDate>Wed, 06 Jul 2022 12:37:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-AB-Swap-without-HSE/m-p/1485416#M16227</guid>
      <dc:creator>ValTek</dc:creator>
      <dc:date>2022-07-06T12:37:24Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 AB Swap without HSE</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-AB-Swap-without-HSE/m-p/1487921#M16304</link>
      <description>&lt;P&gt;Hi Vincenzo,&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;No, AB Swap is supported only with HSE. You can download HSE FW and HSE demo app, HSE OTADEMO from S32K3 Standard Software and S32K3 Reference Software packages:&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-STDSW-D" target="_blank"&gt;https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-STDSW-D&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D" target="_blank"&gt;https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D&lt;/A&gt;&lt;/P&gt;
&lt;OL start="2"&gt;
&lt;LI&gt;No, that’s not possible.&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jul 2022 07:45:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-AB-Swap-without-HSE/m-p/1487921#M16304</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-07-12T07:45:33Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 AB Swap without HSE</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-AB-Swap-without-HSE/m-p/1529958#M18044</link>
      <description>&lt;P&gt;hi lucas,&lt;/P&gt;&lt;P&gt;Can you tell me that where can i download the SW32K3_OTADEMO_0.8.0_D2203?&lt;/P&gt;&lt;P&gt;thanks a lot.&lt;/P&gt;</description>
      <pubDate>Thu, 29 Sep 2022 02:16:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-AB-Swap-without-HSE/m-p/1529958#M18044</guid>
      <dc:creator>PatrickPP</dc:creator>
      <dc:date>2022-09-29T02:16:27Z</dc:date>
    </item>
  </channel>
</rss>