<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: AN5320 soft in S32K</title>
    <link>https://community.nxp.com/t5/S32K/AN5320-soft/m-p/1529179#M18026</link>
    <description>&lt;P&gt;Hi&amp;nbsp;lengrudie,&lt;/P&gt;
&lt;P&gt;There is no &lt;A href="https://www.nxp.com/docs/en/application-note/AN5320.pdf" target="_blank" rel="noopener noreferrer"&gt;&lt;SPAN&gt;Using LPSPI on KL28Z&lt;/SPAN&gt;&lt;/A&gt;&amp;nbsp; AN5320SW, so you can not find it. The code is shown in this AN.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Wed, 28 Sep 2022 03:51:21 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2022-09-28T03:51:21Z</dc:date>
    <item>
      <title>AN5320 soft</title>
      <link>https://community.nxp.com/t5/S32K/AN5320-soft/m-p/1529093#M18020</link>
      <description>&lt;P&gt;How can I fine AN5320 demo?&lt;/P&gt;</description>
      <pubDate>Wed, 28 Sep 2022 01:14:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/AN5320-soft/m-p/1529093#M18020</guid>
      <dc:creator>lengrudie</dc:creator>
      <dc:date>2022-09-28T01:14:45Z</dc:date>
    </item>
    <item>
      <title>Re: AN5320 soft</title>
      <link>https://community.nxp.com/t5/S32K/AN5320-soft/m-p/1529179#M18026</link>
      <description>&lt;P&gt;Hi&amp;nbsp;lengrudie,&lt;/P&gt;
&lt;P&gt;There is no &lt;A href="https://www.nxp.com/docs/en/application-note/AN5320.pdf" target="_blank" rel="noopener noreferrer"&gt;&lt;SPAN&gt;Using LPSPI on KL28Z&lt;/SPAN&gt;&lt;/A&gt;&amp;nbsp; AN5320SW, so you can not find it. The code is shown in this AN.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 28 Sep 2022 03:51:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/AN5320-soft/m-p/1529179#M18026</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-09-28T03:51:21Z</dc:date>
    </item>
  </channel>
</rss>