<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K RTC Demo Bug in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K-RTC-Demo-Bug/m-p/727963#M1794</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The LPOCLKS[RTCCLKSEL] register is a write-once register.&lt;/P&gt;&lt;P&gt;It is reset only on POR or LVD.&lt;/P&gt;&lt;P&gt;So please run the code from Flash, not RAM, and power-on reset the MCU.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Mar 2018 13:19:28 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2018-03-09T13:19:28Z</dc:date>
    <item>
      <title>S32K RTC Demo Bug</title>
      <link>https://community.nxp.com/t5/S32K/S32K-RTC-Demo-Bug/m-p/727962#M1793</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have imported Demo project "rtc_alarm_s32k144" to&amp;nbsp;S32DS ,However ,I found the Interrupt peroid is not 1 second in function "secondsISR()", Actually it is far less than 1 second。&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38290i4CA3316F3F70A83F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the other way, it will work well if i change ".clockSelect" to&amp;nbsp;RTC_CLK_SRC_LPO_1KHZ, as below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/37929i86F1E9B8EDF671DC/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can somebody tell me why? Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Mar 2018 10:52:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-RTC-Demo-Bug/m-p/727962#M1793</guid>
      <dc:creator>kawadaxi</dc:creator>
      <dc:date>2018-03-05T10:52:58Z</dc:date>
    </item>
    <item>
      <title>Re: S32K RTC Demo Bug</title>
      <link>https://community.nxp.com/t5/S32K/S32K-RTC-Demo-Bug/m-p/727963#M1794</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The LPOCLKS[RTCCLKSEL] register is a write-once register.&lt;/P&gt;&lt;P&gt;It is reset only on POR or LVD.&lt;/P&gt;&lt;P&gt;So please run the code from Flash, not RAM, and power-on reset the MCU.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Mar 2018 13:19:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-RTC-Demo-Bug/m-p/727963#M1794</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-03-09T13:19:28Z</dc:date>
    </item>
  </channel>
</rss>