<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックProblem with unified bootloader S32k344</title>
    <link>https://community.nxp.com/t5/S32K/Problem-with-unified-bootloader-S32k344/m-p/1524310#M17800</link>
    <description>&lt;P&gt;Hi !&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to update this demo to RTD 2.0 Version.&lt;/P&gt;&lt;P&gt;I changed the SDK and i change the library directory, and the sdk.&lt;/P&gt;&lt;P&gt;But when i try to update the code i always have the same error:&amp;nbsp;&lt;/P&gt;&lt;P&gt;Issue: Processor '' detected in NXP GCC 10.2 for Arm 32-bit Bare-Metal project does not match with currently selected 'S32K344'. Target processor not supported or the computer is not on-line.&lt;BR /&gt;Level: Error&lt;BR /&gt;Type: Tool problem&lt;BR /&gt;Tool: McuConfiguration&lt;BR /&gt;Origin: S32K344_CAN_Bootloader_RTD100&lt;BR /&gt;Resource: Processor&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;I dont know what i can see to resolve this error .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Miguel&lt;/P&gt;</description>
    <pubDate>Wed, 21 Sep 2022 08:18:37 GMT</pubDate>
    <dc:creator>Miki849</dc:creator>
    <dc:date>2022-09-21T08:18:37Z</dc:date>
    <item>
      <title>Problem with unified bootloader S32k344</title>
      <link>https://community.nxp.com/t5/S32K/Problem-with-unified-bootloader-S32k344/m-p/1524310#M17800</link>
      <description>&lt;P&gt;Hi !&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to update this demo to RTD 2.0 Version.&lt;/P&gt;&lt;P&gt;I changed the SDK and i change the library directory, and the sdk.&lt;/P&gt;&lt;P&gt;But when i try to update the code i always have the same error:&amp;nbsp;&lt;/P&gt;&lt;P&gt;Issue: Processor '' detected in NXP GCC 10.2 for Arm 32-bit Bare-Metal project does not match with currently selected 'S32K344'. Target processor not supported or the computer is not on-line.&lt;BR /&gt;Level: Error&lt;BR /&gt;Type: Tool problem&lt;BR /&gt;Tool: McuConfiguration&lt;BR /&gt;Origin: S32K344_CAN_Bootloader_RTD100&lt;BR /&gt;Resource: Processor&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;I dont know what i can see to resolve this error .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Miguel&lt;/P&gt;</description>
      <pubDate>Wed, 21 Sep 2022 08:18:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-with-unified-bootloader-S32k344/m-p/1524310#M17800</guid>
      <dc:creator>Miki849</dc:creator>
      <dc:date>2022-09-21T08:18:37Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with unified bootloader S32k344</title>
      <link>https://community.nxp.com/t5/S32K/Problem-with-unified-bootloader-S32k344/m-p/1525984#M17870</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/194612"&gt;@Miki849&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;Try the following:&lt;BR /&gt;Using Project wizard, create a new project, selecting S32K3 device, and the new SDK in the SDK selection menu.&lt;/LI&gt;
&lt;LI&gt;Copy the application source files from your pre-existing project as well as any customizations you made to the project properties.\&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;Note: If you used the S32 Configuration Tools to setup pins, clocks, peripherals, etc. These settings could be exported from the existing project and then imported into the new one.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope this will help you.&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Wed, 21 Sep 2022 15:45:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-with-unified-bootloader-S32k344/m-p/1525984#M17870</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2022-09-21T15:45:42Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with unified bootloader S32k344</title>
      <link>https://community.nxp.com/t5/S32K/Problem-with-unified-bootloader-S32k344/m-p/1798238#M31236</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/194612"&gt;@Miki849&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi Miguel, I am getting the same error message as you had pointed out. I am getting the Error in a different context but not in bootloader.&lt;/P&gt;&lt;P&gt;I get the error message:&amp;nbsp;&lt;STRONG&gt;Processor "" detected in the NXP GCC 10.2 for Arm 32 bit Bare-Metal project does not match the currently selected "S32K344".&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Were you able to resolve this error? I am not sure what mistake I have done in the project.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I have posted the issue here:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/S32K3xx-Error-in-S32DS-Platform-IDE-while-configuring-the/m-p/1797624#M31207" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K3xx-Error-in-S32DS-Platform-IDE-while-configuring-the/m-p/1797624#M31207&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jan 2024 03:59:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-with-unified-bootloader-S32k344/m-p/1798238#M31236</guid>
      <dc:creator>tecprasant</dc:creator>
      <dc:date>2024-01-31T03:59:04Z</dc:date>
    </item>
  </channel>
</rss>