<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K144 DAC CMP0_out</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-DAC-CMP0-out/m-p/1521402#M17684</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I need an analog signal (0V to 10V) on pin 18 of the FS32K144 LQFP100 processor.&lt;/P&gt;&lt;P&gt;The configuration options for this pin are: FTM0_FLT0, LPUART2_RTS, FTM2_FLT0, TRGMUX_IN6 and CMP0_OUT.&lt;/P&gt;&lt;P&gt;Is it possible to use CMP0_OUT as an analog output?&lt;/P&gt;</description>
    <pubDate>Tue, 13 Sep 2022 18:16:06 GMT</pubDate>
    <dc:creator>dsilva</dc:creator>
    <dc:date>2022-09-13T18:16:06Z</dc:date>
    <item>
      <title>S32K144 DAC CMP0_out</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-DAC-CMP0-out/m-p/1521402#M17684</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I need an analog signal (0V to 10V) on pin 18 of the FS32K144 LQFP100 processor.&lt;/P&gt;&lt;P&gt;The configuration options for this pin are: FTM0_FLT0, LPUART2_RTS, FTM2_FLT0, TRGMUX_IN6 and CMP0_OUT.&lt;/P&gt;&lt;P&gt;Is it possible to use CMP0_OUT as an analog output?&lt;/P&gt;</description>
      <pubDate>Tue, 13 Sep 2022 18:16:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-DAC-CMP0-out/m-p/1521402#M17684</guid>
      <dc:creator>dsilva</dc:creator>
      <dc:date>2022-09-13T18:16:06Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 DAC CMP0_out</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-DAC-CMP0-out/m-p/1521675#M17690</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;The DAC from a comparator is available as an on-chip internal signal only and is &lt;STRONG&gt;not&lt;/STRONG&gt; available externally to a pin.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="45.2 Introduction.png" style="width: 903px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/193552i2D22656D21B361D5/image-size/large?v=v2&amp;amp;px=999" role="button" title="45.2 Introduction.png" alt="45.2 Introduction.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Figure 45-1. CMP high level diagram.png" style="width: 877px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/193551i7EA6561AA6AD4259/image-size/large?v=v2&amp;amp;px=999" role="button" title="Figure 45-1. CMP high level diagram.png" alt="Figure 45-1. CMP high level diagram.png" /&gt;&lt;/span&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 14 Sep 2022 05:50:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-DAC-CMP0-out/m-p/1521675#M17690</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-09-14T05:50:37Z</dc:date>
    </item>
  </channel>
</rss>