<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K3xx - media clock timestamping using PPS0 input</title>
    <link>https://community.nxp.com/t5/S32K/S32K3xx-media-clock-timestamping-using-PPS0-input/m-p/1521236#M17673</link>
    <description>&lt;P&gt;Hello. Is there any update here?&lt;/P&gt;</description>
    <pubDate>Tue, 13 Sep 2022 11:43:29 GMT</pubDate>
    <dc:creator>jakub_mielczare</dc:creator>
    <dc:date>2022-09-13T11:43:29Z</dc:date>
    <item>
      <title>S32K3xx - media clock timestamping using PPS0 input</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-media-clock-timestamping-using-PPS0-input/m-p/1469305#M15798</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In S32K3 RM, in chapter "73.17.167 MAC PPS Control (MAC_PPS_Control)" it says that PPS0 can be used to capture presentation time at rising/falling/both edge of a media clock.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Selection_631.png" style="width: 970px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/182297i6836FB1419822F01/image-size/large?v=v2&amp;amp;px=999" role="button" title="Selection_631.png" alt="Selection_631.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Selection_631.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But the same values of PPSCTRL_PPS CMD are used also above in the manual:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Selection_632.png" style="width: 837px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/182298iF764859D508DD80B/image-size/large?v=v2&amp;amp;px=999" role="button" title="Selection_632.png" alt="Selection_632.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Selection_632.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How is it defined which of the above value sets are effective, pulse train or timestamp capture on edge?&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Jakub&lt;/P&gt;</description>
      <pubDate>Mon, 06 Jun 2022 10:08:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-media-clock-timestamping-using-PPS0-input/m-p/1469305#M15798</guid>
      <dc:creator>jakub_mielczare</dc:creator>
      <dc:date>2022-06-06T10:08:35Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3xx - media clock timestamping using PPS0 input</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-media-clock-timestamping-using-PPS0-input/m-p/1471302#M15866</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hi&amp;nbsp;Jakub,&lt;/P&gt;
&lt;P&gt;The attachment is a draft version of PPS user guide. You can refer to it.&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Shuang&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jun 2022 08:14:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-media-clock-timestamping-using-PPS0-input/m-p/1471302#M15866</guid>
      <dc:creator>Shuang</dc:creator>
      <dc:date>2022-06-09T08:14:50Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3xx - media clock timestamping using PPS0 input</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-media-clock-timestamping-using-PPS0-input/m-p/1513271#M17372</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you for the answer and the PPT file.&lt;/P&gt;&lt;P&gt;Is it possible to read timestamps from MAC PPS0 Target Time registers (written by MAC on capturing rising/falling edge of an external clock signal) by CPU or only DMA can make those reads?&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Jakub&lt;/P&gt;</description>
      <pubDate>Mon, 29 Aug 2022 15:34:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-media-clock-timestamping-using-PPS0-input/m-p/1513271#M17372</guid>
      <dc:creator>jakub_mielczare</dc:creator>
      <dc:date>2022-08-29T15:34:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3xx - media clock timestamping using PPS0 input</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-media-clock-timestamping-using-PPS0-input/m-p/1521236#M17673</link>
      <description>&lt;P&gt;Hello. Is there any update here?&lt;/P&gt;</description>
      <pubDate>Tue, 13 Sep 2022 11:43:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-media-clock-timestamping-using-PPS0-input/m-p/1521236#M17673</guid>
      <dc:creator>jakub_mielczare</dc:creator>
      <dc:date>2022-09-13T11:43:29Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3xx - media clock timestamping using PPS0 input</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-media-clock-timestamping-using-PPS0-input/m-p/1521237#M17674</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Is there any update in this topic?&lt;/P&gt;</description>
      <pubDate>Tue, 13 Sep 2022 11:44:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-media-clock-timestamping-using-PPS0-input/m-p/1521237#M17674</guid>
      <dc:creator>jakub_mielczare</dc:creator>
      <dc:date>2022-09-13T11:44:27Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3xx - media clock timestamping using PPS0 input</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-media-clock-timestamping-using-PPS0-input/m-p/1521596#M17687</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hi&amp;nbsp;Jakub,CPU and DMA can read&amp;amp;write MAC PPS0 Target Time registers. DMA can reduce CPU loading and it is recommended for operation.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The attachment is a demo project that DMA will write data to&amp;nbsp;MAC PPS0 Target Time registers and will generate media clock.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Shuang&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Sep 2022 03:23:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-media-clock-timestamping-using-PPS0-input/m-p/1521596#M17687</guid>
      <dc:creator>Shuang</dc:creator>
      <dc:date>2022-09-14T03:23:33Z</dc:date>
    </item>
  </channel>
</rss>