<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K lwip_S32K148 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K-lwip-S32K148/m-p/1515666#M17460</link>
    <description>&lt;P&gt;Hello NXP Community,&lt;/P&gt;&lt;P&gt;I run the the project lwip_S32K148 , it works, I can ping 192.168.0.200 via cmd. But how can I use the driver enet in this project to use ENET_DRV_ReadFrame/ENET_DRV_SendFrame. I need to send/receive the datas by TCP/IP from PC and&amp;nbsp; after send/receive to another board by UART.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;</description>
    <pubDate>Thu, 01 Sep 2022 14:39:58 GMT</pubDate>
    <dc:creator>Alex19</dc:creator>
    <dc:date>2022-09-01T14:39:58Z</dc:date>
    <item>
      <title>S32K lwip_S32K148</title>
      <link>https://community.nxp.com/t5/S32K/S32K-lwip-S32K148/m-p/1515666#M17460</link>
      <description>&lt;P&gt;Hello NXP Community,&lt;/P&gt;&lt;P&gt;I run the the project lwip_S32K148 , it works, I can ping 192.168.0.200 via cmd. But how can I use the driver enet in this project to use ENET_DRV_ReadFrame/ENET_DRV_SendFrame. I need to send/receive the datas by TCP/IP from PC and&amp;nbsp; after send/receive to another board by UART.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;</description>
      <pubDate>Thu, 01 Sep 2022 14:39:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-lwip-S32K148/m-p/1515666#M17460</guid>
      <dc:creator>Alex19</dc:creator>
      <dc:date>2022-09-01T14:39:58Z</dc:date>
    </item>
    <item>
      <title>Re: S32K lwip_S32K148</title>
      <link>https://community.nxp.com/t5/S32K/S32K-lwip-S32K148/m-p/1516967#M17532</link>
      <description>&lt;P&gt;Hi &lt;SPAN class="test-id__field-value slds-form-element__static slds-grow word-break-ie11"&gt;Aleksandr&lt;/SPAN&gt;,&lt;/P&gt;
&lt;P&gt;If you want to use TCP IP layer, please check documentation of LWIP stack.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nongnu.org/lwip/2_0_x/index.html" target="_blank"&gt;https://www.nongnu.org/lwip/2_0_x/index.html&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Notice that LWIP is open source software, so we provide only very limited support.&lt;/P&gt;
&lt;P&gt;ENET_DRV... belongs to data link layer which is described in SDK user manual:&lt;/P&gt;
&lt;P&gt;c:\NXP\S32DS.3.4\S32DS\software\S32SDK_S32K1XX_RTM_4.0.2\doc\S32SDK_S32K148_UserManual.pdf&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Mon, 05 Sep 2022 10:09:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-lwip-S32K148/m-p/1516967#M17532</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-09-05T10:09:28Z</dc:date>
    </item>
  </channel>
</rss>