<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic V15 for S32K344 is about 0.2V while using BJT in S32K</title>
    <link>https://community.nxp.com/t5/S32K/V15-for-S32K344-is-about-0-2V-while-using-BJT/m-p/1514443#M17424</link>
    <description>&lt;P&gt;my client made a S32K344 board ,the&amp;nbsp;V15 is power by a BJT , but the voltage for V15 is about 0.2V while the PET13 is 0 voltage.&lt;/P&gt;&lt;P&gt;i checked the EVK the V15 is about 0.1V and the PET13 is 0 voltage.&lt;/P&gt;&lt;P&gt;can anyone help me ?&lt;/P&gt;</description>
    <pubDate>Wed, 31 Aug 2022 07:33:46 GMT</pubDate>
    <dc:creator>steven_zhang</dc:creator>
    <dc:date>2022-08-31T07:33:46Z</dc:date>
    <item>
      <title>V15 for S32K344 is about 0.2V while using BJT</title>
      <link>https://community.nxp.com/t5/S32K/V15-for-S32K344-is-about-0-2V-while-using-BJT/m-p/1514443#M17424</link>
      <description>&lt;P&gt;my client made a S32K344 board ,the&amp;nbsp;V15 is power by a BJT , but the voltage for V15 is about 0.2V while the PET13 is 0 voltage.&lt;/P&gt;&lt;P&gt;i checked the EVK the V15 is about 0.1V and the PET13 is 0 voltage.&lt;/P&gt;&lt;P&gt;can anyone help me ?&lt;/P&gt;</description>
      <pubDate>Wed, 31 Aug 2022 07:33:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/V15-for-S32K344-is-about-0-2V-while-using-BJT/m-p/1514443#M17424</guid>
      <dc:creator>steven_zhang</dc:creator>
      <dc:date>2022-08-31T07:33:46Z</dc:date>
    </item>
    <item>
      <title>Re: V15 for S32K344 is about 0.2V while using BJT</title>
      <link>https://community.nxp.com/t5/S32K/V15-for-S32K344-is-about-0-2V-while-using-BJT/m-p/1516086#M17477</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/7131"&gt;@steven_zhang&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Is the &lt;STRONG&gt;LMBCTLEN&lt;/STRONG&gt; bit set?&lt;/P&gt;
&lt;P&gt;Please refer to &lt;STRONG&gt;Figure 159. Last-mile regulator enable sequence&lt;/STRONG&gt; in the RM, rev.4&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Fri, 02 Sep 2022 07:31:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/V15-for-S32K344-is-about-0-2V-while-using-BJT/m-p/1516086#M17477</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2022-09-02T07:31:13Z</dc:date>
    </item>
    <item>
      <title>Re: V15 for S32K344 is about 0.2V while using BJT</title>
      <link>https://community.nxp.com/t5/S32K/V15-for-S32K344-is-about-0-2V-while-using-BJT/m-p/1516131#M17480</link>
      <description>&lt;P&gt;i found the power_1 module in which one can config the regulater.&lt;/P&gt;</description>
      <pubDate>Fri, 02 Sep 2022 08:29:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/V15-for-S32K344-is-about-0-2V-while-using-BJT/m-p/1516131#M17480</guid>
      <dc:creator>steven_zhang</dc:creator>
      <dc:date>2022-09-02T08:29:02Z</dc:date>
    </item>
  </channel>
</rss>