<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can I use MC33664 with RaspberryPi ? in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Can-I-use-MC33664-with-RaspberryPi/m-p/1513614#M17387</link>
    <description>&lt;P&gt;Thanks a lot sir,&lt;/P&gt;&lt;P&gt;I read somewhere that the Raspberry pi can't be configured as a slave (about SPI I mean), is it a problem ?&lt;/P&gt;&lt;P&gt;I only want to read cells voltages&lt;/P&gt;</description>
    <pubDate>Tue, 30 Aug 2022 06:13:13 GMT</pubDate>
    <dc:creator>Yan1</dc:creator>
    <dc:date>2022-08-30T06:13:13Z</dc:date>
    <item>
      <title>Can I use MC33664 with RaspberryPi ?</title>
      <link>https://community.nxp.com/t5/S32K/Can-I-use-MC33664-with-RaspberryPi/m-p/1513083#M17364</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;I have a battery with 14 cells equipped with a MC3377x using TPL communication.&lt;BR /&gt;Can I use the MC33664 component with a raspberry pi zith SPI to read the 14 cells voltages ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Yan&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 29 Aug 2022 10:09:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-I-use-MC33664-with-RaspberryPi/m-p/1513083#M17364</guid>
      <dc:creator>Yan1</dc:creator>
      <dc:date>2022-08-29T10:09:36Z</dc:date>
    </item>
    <item>
      <title>Re: Can I use MC33664 with RaspberryPi ?</title>
      <link>https://community.nxp.com/t5/S32K/Can-I-use-MC33664-with-RaspberryPi/m-p/1513563#M17381</link>
      <description>&lt;P&gt;Hi Yan,&lt;/P&gt;
&lt;P&gt;yes, you can use any microcontroller with two SPI modules and with 3.3V / 5V compatible logic thresholds.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Tue, 30 Aug 2022 04:55:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-I-use-MC33664-with-RaspberryPi/m-p/1513563#M17381</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-08-30T04:55:58Z</dc:date>
    </item>
    <item>
      <title>Re: Can I use MC33664 with RaspberryPi ?</title>
      <link>https://community.nxp.com/t5/S32K/Can-I-use-MC33664-with-RaspberryPi/m-p/1513614#M17387</link>
      <description>&lt;P&gt;Thanks a lot sir,&lt;/P&gt;&lt;P&gt;I read somewhere that the Raspberry pi can't be configured as a slave (about SPI I mean), is it a problem ?&lt;/P&gt;&lt;P&gt;I only want to read cells voltages&lt;/P&gt;</description>
      <pubDate>Tue, 30 Aug 2022 06:13:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-I-use-MC33664-with-RaspberryPi/m-p/1513614#M17387</guid>
      <dc:creator>Yan1</dc:creator>
      <dc:date>2022-08-30T06:13:13Z</dc:date>
    </item>
    <item>
      <title>Re: Can I use MC33664 with RaspberryPi ?</title>
      <link>https://community.nxp.com/t5/S32K/Can-I-use-MC33664-with-RaspberryPi/m-p/1513677#M17392</link>
      <description>&lt;P&gt;Yes, that will be a problem. You need SPI slave to read data from MC33664.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/MC33664-with-single-SPI-port-on-MCU/m-p/1450883#M15205" target="_blank"&gt;https://community.nxp.com/t5/S32K/MC33664-with-single-SPI-port-on-MCU/m-p/1450883#M15205&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Tue, 30 Aug 2022 07:18:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-I-use-MC33664-with-RaspberryPi/m-p/1513677#M17392</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-08-30T07:18:44Z</dc:date>
    </item>
    <item>
      <title>Re: Can I use MC33664 with RaspberryPi ?</title>
      <link>https://community.nxp.com/t5/S32K/Can-I-use-MC33664-with-RaspberryPi/m-p/1513832#M17408</link>
      <description>&lt;P&gt;So I will try with Arduino instead.&lt;/P&gt;&lt;P&gt;I'm not very good with programming in this field, where can I find (or can you provide) a basic code to use with arduino for reading cells voltages only?&lt;/P&gt;&lt;P&gt;thanks a lot again&lt;/P&gt;</description>
      <pubDate>Tue, 30 Aug 2022 10:17:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-I-use-MC33664-with-RaspberryPi/m-p/1513832#M17408</guid>
      <dc:creator>Yan1</dc:creator>
      <dc:date>2022-08-30T10:17:39Z</dc:date>
    </item>
    <item>
      <title>Re: Can I use MC33664 with RaspberryPi ?</title>
      <link>https://community.nxp.com/t5/S32K/Can-I-use-MC33664-with-RaspberryPi/m-p/1514724#M17434</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a new question to complet previous one.&lt;/P&gt;&lt;P&gt;If I have 2 arduino, Can I use one, configured as a master, to send the message "READ" to the MC33664 (using &lt;SPAN&gt;SCLK_TX, &lt;/SPAN&gt;&lt;SPAN&gt;CSB_TX,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;D&lt;/SPAN&gt;&lt;SPAN&gt;A&lt;/SPAN&gt;&lt;SPAN&gt;T&lt;/SPAN&gt;&lt;SPAN&gt;A&lt;/SPAN&gt;&lt;SPAN&gt;_&lt;/SPAN&gt;&lt;SPAN&gt;T&lt;/SPAN&gt;&lt;SPAN&gt;X I/O)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;and use another Arduino, configured as a slave, to get the response from the MC33664&amp;nbsp; (using&amp;nbsp;&lt;SPAN&gt;CLK_RX, CSB_RX, DATA_RX I/O)&lt;/SPAN&gt; ?&lt;/P&gt;</description>
      <pubDate>Wed, 31 Aug 2022 15:02:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-I-use-MC33664-with-RaspberryPi/m-p/1514724#M17434</guid>
      <dc:creator>Yan1</dc:creator>
      <dc:date>2022-08-31T15:02:42Z</dc:date>
    </item>
    <item>
      <title>Re: Can I use MC33664 with RaspberryPi ?</title>
      <link>https://community.nxp.com/t5/S32K/Can-I-use-MC33664-with-RaspberryPi/m-p/1516054#M17474</link>
      <description>&lt;P&gt;We provide generic driver written in C which can be ported to any suitable 32bit microcontroller. It was tested on S32K144 microcontroller. You can find the software package on this page:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/power-management/battery-management/battery-cell-controllers/14-channel-li-ion-battery-cell-controller-ic:MC33771B" target="_blank"&gt;https://www.nxp.com/products/power-management/battery-management/battery-cell-controllers/14-channel-li-ion-battery-cell-controller-ic:MC33771B&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;… in section Software – Secure files.&lt;/P&gt;
&lt;P&gt;“MC33771B&amp;amp;MC33772B Battery Cell Controllers - Software Driver”&lt;/P&gt;
&lt;P&gt;Direct link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/sd/collateral/1644518515884709073509?version=1.1" target="_blank"&gt;https://www.nxp.com/webapp/sd/collateral/1644518515884709073509?version=1.1&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;In case you do not have an access:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/nxp-secure-access-rights-registration.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/nxp-secure-access-rights-registration.pdf&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 02 Sep 2022 07:00:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-I-use-MC33664-with-RaspberryPi/m-p/1516054#M17474</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-09-02T07:00:54Z</dc:date>
    </item>
    <item>
      <title>Re: Can I use MC33664 with RaspberryPi ?</title>
      <link>https://community.nxp.com/t5/S32K/Can-I-use-MC33664-with-RaspberryPi/m-p/1516056#M17475</link>
      <description>&lt;P&gt;Yes, that's also possible.&lt;/P&gt;</description>
      <pubDate>Fri, 02 Sep 2022 07:01:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-I-use-MC33664-with-RaspberryPi/m-p/1516056#M17475</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-09-02T07:01:17Z</dc:date>
    </item>
  </channel>
</rss>