<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic The problem of using LPUART in s32k144 with FreeRTOS in S32K</title>
    <link>https://community.nxp.com/t5/S32K/The-problem-of-using-LPUART-in-s32k144-with-FreeRTOS/m-p/1512719#M17349</link>
    <description>&lt;P&gt;If don't use freeRTOS , The function LPUART_DRV_SendDataBlocking(INST_LPUART1, (uint8_t *)str, strlen(str), UART_TIMEOUT) works well. But if import freeRTOS to project , this function only tx the first one byte, and never back.&lt;BR /&gt;even I set the priority of LPUART1_RxTx_IRQn bigger then configMAX_SYSCALL_INTERRUPT_PRIORITY ,&amp;nbsp; but it still send only one byte.&lt;/P&gt;&lt;P&gt;The init code :&lt;BR /&gt;/* Initialize LPUART instance */&lt;BR /&gt;LPUART_DRV_Init(INST_LPUART1, &amp;amp;lpuart1_State, &amp;amp;lpuart1_InitConfig0);&lt;/P&gt;&lt;P&gt;INT_SYS_SetPriority(LPUART1_RxTx_IRQn,configMAX_SYSCALL_INTERRUPT_PRIORITY + 2 );&lt;BR /&gt;INT_SYS_EnableIRQ(LPUART1_RxTx_IRQn);&lt;/P&gt;&lt;P&gt;Thanks !&lt;/P&gt;</description>
    <pubDate>Sun, 28 Aug 2022 04:09:32 GMT</pubDate>
    <dc:creator>zhangxujun1981</dc:creator>
    <dc:date>2022-08-28T04:09:32Z</dc:date>
    <item>
      <title>The problem of using LPUART in s32k144 with FreeRTOS</title>
      <link>https://community.nxp.com/t5/S32K/The-problem-of-using-LPUART-in-s32k144-with-FreeRTOS/m-p/1512719#M17349</link>
      <description>&lt;P&gt;If don't use freeRTOS , The function LPUART_DRV_SendDataBlocking(INST_LPUART1, (uint8_t *)str, strlen(str), UART_TIMEOUT) works well. But if import freeRTOS to project , this function only tx the first one byte, and never back.&lt;BR /&gt;even I set the priority of LPUART1_RxTx_IRQn bigger then configMAX_SYSCALL_INTERRUPT_PRIORITY ,&amp;nbsp; but it still send only one byte.&lt;/P&gt;&lt;P&gt;The init code :&lt;BR /&gt;/* Initialize LPUART instance */&lt;BR /&gt;LPUART_DRV_Init(INST_LPUART1, &amp;amp;lpuart1_State, &amp;amp;lpuart1_InitConfig0);&lt;/P&gt;&lt;P&gt;INT_SYS_SetPriority(LPUART1_RxTx_IRQn,configMAX_SYSCALL_INTERRUPT_PRIORITY + 2 );&lt;BR /&gt;INT_SYS_EnableIRQ(LPUART1_RxTx_IRQn);&lt;/P&gt;&lt;P&gt;Thanks !&lt;/P&gt;</description>
      <pubDate>Sun, 28 Aug 2022 04:09:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/The-problem-of-using-LPUART-in-s32k144-with-FreeRTOS/m-p/1512719#M17349</guid>
      <dc:creator>zhangxujun1981</dc:creator>
      <dc:date>2022-08-28T04:09:32Z</dc:date>
    </item>
    <item>
      <title>Re: The problem of using LPUART in s32k144 with FreeRTOS</title>
      <link>https://community.nxp.com/t5/S32K/The-problem-of-using-LPUART-in-s32k144-with-FreeRTOS/m-p/1513076#M17363</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205595"&gt;@zhangxujun1981&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;It was discussed in this thread:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-SDK/Send-Data-using-Blocking-method-within-FreeRTOS-Fail/td-p/1425999" target="_blank"&gt;https://community.nxp.com/t5/S32-SDK/Send-Data-using-Blocking-method-within-FreeRTOS-Fail/td-p/1425999&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please have a look.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 29 Aug 2022 10:01:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/The-problem-of-using-LPUART-in-s32k144-with-FreeRTOS/m-p/1513076#M17363</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2022-08-29T10:01:07Z</dc:date>
    </item>
    <item>
      <title>Re: The problem of using LPUART in s32k144 with FreeRTOS</title>
      <link>https://community.nxp.com/t5/S32K/The-problem-of-using-LPUART-in-s32k144-with-FreeRTOS/m-p/1515235#M17441</link>
      <description>&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Thu, 01 Sep 2022 05:33:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/The-problem-of-using-LPUART-in-s32k144-with-FreeRTOS/m-p/1515235#M17441</guid>
      <dc:creator>zhangxujun1981</dc:creator>
      <dc:date>2022-09-01T05:33:06Z</dc:date>
    </item>
  </channel>
</rss>