<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Can S32K144 internal RTC wake up itself in VLPR or VLPS mode?</title>
    <link>https://community.nxp.com/t5/S32K/Can-S32K144-internal-RTC-wake-up-itself-in-VLPR-or-VLPS-mode/m-p/723697#M1733</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Daniel,&lt;/P&gt;&lt;P&gt;to my understanding this will change with the documentation update end of Jan next year&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Jochen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Nov 2017 14:04:21 GMT</pubDate>
    <dc:creator>jochengerster</dc:creator>
    <dc:date>2017-11-27T14:04:21Z</dc:date>
    <item>
      <title>Can S32K144 internal RTC wake up itself in VLPR or VLPS mode?</title>
      <link>https://community.nxp.com/t5/S32K/Can-S32K144-internal-RTC-wake-up-itself-in-VLPR-or-VLPS-mode/m-p/723695#M1731</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi：&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;Can&amp;nbsp;S32K144 internal RTC wake up itself in VLPR or VLPS mode?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; What's the meaning of "The wakeup pin is not available for RTC on this device"?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/34300iE90584A8A0A74443/image-size/large?v=v2&amp;amp;px=999" title="RTC.PNG" alt="RTC.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Nov 2017 02:52:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-S32K144-internal-RTC-wake-up-itself-in-VLPR-or-VLPS-mode/m-p/723695#M1731</guid>
      <dc:creator>maoyuanluo</dc:creator>
      <dc:date>2017-11-22T02:52:05Z</dc:date>
    </item>
    <item>
      <title>Re: Can S32K144 internal RTC wake up itself in VLPR or VLPS mode?</title>
      <link>https://community.nxp.com/t5/S32K/Can-S32K144-internal-RTC-wake-up-itself-in-VLPR-or-VLPS-mode/m-p/723696#M1732</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The RTC module doesn’t wake up from VLPS, only from STOP1/2 modes. And it is functional in VLPR.&lt;/P&gt;&lt;P&gt;Please refer to Chapter 7.3.1 (Wake-up sources) and Table 35-4 (Module operation in available low power modes).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The wakeup pin is asserted when a RTC interrupt occurs.&lt;/P&gt;&lt;P&gt;But this pin is not available on S32K1xx.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Nov 2017 16:07:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-S32K144-internal-RTC-wake-up-itself-in-VLPR-or-VLPS-mode/m-p/723696#M1732</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-11-22T16:07:16Z</dc:date>
    </item>
    <item>
      <title>Re: Can S32K144 internal RTC wake up itself in VLPR or VLPS mode?</title>
      <link>https://community.nxp.com/t5/S32K/Can-S32K144-internal-RTC-wake-up-itself-in-VLPR-or-VLPS-mode/m-p/723697#M1733</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Daniel,&lt;/P&gt;&lt;P&gt;to my understanding this will change with the documentation update end of Jan next year&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Jochen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Nov 2017 14:04:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-S32K144-internal-RTC-wake-up-itself-in-VLPR-or-VLPS-mode/m-p/723697#M1733</guid>
      <dc:creator>jochengerster</dc:creator>
      <dc:date>2017-11-27T14:04:21Z</dc:date>
    </item>
  </channel>
</rss>