<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ISELED without EVB in S32K</title>
    <link>https://community.nxp.com/t5/S32K/ISELED-without-EVB/m-p/1511727#M17313</link>
    <description>&lt;P&gt;Hi Cristian,&lt;/P&gt;
&lt;P&gt;Yes, as you can see in FACT SHEET S32K ISELED&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/fact-sheet/S32K-ISELED-FS.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/fact-sheet/S32K-ISELED-FS.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;For production, developers should order one of the S32K ISELED part numbers&lt;BR /&gt;below which include the full production license with unlimited driver functionality.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 25 Aug 2022 11:23:34 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2022-08-25T11:23:34Z</dc:date>
    <item>
      <title>ISELED without EVB</title>
      <link>https://community.nxp.com/t5/S32K/ISELED-without-EVB/m-p/1509677#M17250</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I have tried the S32K144-EVB with ISELED and now I would like to develop my own PCB and try the proper MCU with an integrated iseled interface. But I wanna know if I have to consider other things. For example, when using the evb and SDK it has a maximum number of configurations and then you have to reflash, with the proper MCUs I suppose that there is not a limit, right? is there anything else to consider?&lt;/P&gt;&lt;P&gt;E.g of MCUs with ISELED: FS32K116LIT0VFMT, FS32K118LIT0VLFT, etc.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Cristian&lt;/P&gt;</description>
      <pubDate>Mon, 22 Aug 2022 18:45:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ISELED-without-EVB/m-p/1509677#M17250</guid>
      <dc:creator>cristian20a</dc:creator>
      <dc:date>2022-08-22T18:45:49Z</dc:date>
    </item>
    <item>
      <title>Re: ISELED without EVB</title>
      <link>https://community.nxp.com/t5/S32K/ISELED-without-EVB/m-p/1511727#M17313</link>
      <description>&lt;P&gt;Hi Cristian,&lt;/P&gt;
&lt;P&gt;Yes, as you can see in FACT SHEET S32K ISELED&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/fact-sheet/S32K-ISELED-FS.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/fact-sheet/S32K-ISELED-FS.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;For production, developers should order one of the S32K ISELED part numbers&lt;BR /&gt;below which include the full production license with unlimited driver functionality.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 25 Aug 2022 11:23:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ISELED-without-EVB/m-p/1511727#M17313</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2022-08-25T11:23:34Z</dc:date>
    </item>
  </channel>
</rss>