<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K344 and TJA1101B debugging problems in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-and-TJA1101B-debugging-problems/m-p/1511417#M17303</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Probably there were some jumper problems. You will have to move the jumper J30 on eval board from position 3-4 CLOSED to 1-2 CLOSED in order for on-board Ethernet level shifters to work properly.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Nam&lt;/P&gt;</description>
    <pubDate>Thu, 25 Aug 2022 04:29:53 GMT</pubDate>
    <dc:creator>namnguyenviet</dc:creator>
    <dc:date>2022-08-25T04:29:53Z</dc:date>
    <item>
      <title>S32K344 and TJA1101B debugging problems</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-and-TJA1101B-debugging-problems/m-p/1508555#M17191</link>
      <description>&lt;P&gt;Hi，I'm debugging the Tja1101 using s32k344.&lt;/P&gt;&lt;P&gt;Problem 1：&lt;/P&gt;&lt;P&gt;I config the s32k344 mcal use EB tresos 27. and call the Eth_Transmit() function to send the ARP message in a period of 2s,LED for activity on my media converter keeps blinking in a period of 2s, but I don't see any packets on my PC(wireShark).The media conerter can work well when I use SPC5748G develop board.&lt;/P&gt;&lt;P&gt;I checked the register in TJA1101 through SMI, the register 1 and register 23 showing the&amp;nbsp; LINK UP is OK,and SQI&amp;nbsp; is&amp;nbsp;&amp;nbsp;class G SQI (very good link).PHY STATE is Active,TX_MODE is SEND_N,not any ERR occured, PHY is MII mode and config as Master.&lt;/P&gt;&lt;P&gt;The following figure1 shows the waveforms of TXEN and TXD0 ports captured by the oscilloscope，the TXCLK is 25MHZ. Can you see any problems from the waveforms？&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Problem 2：&lt;/P&gt;&lt;P&gt;I use PC sends an ARP message to s32k344, and the Eth_Receive() callback function Eth_Rxindication() can't receive the message all the time. The waveforms of RXDV and RXD0 can be captured through the oscilloscope ，please refer figure2，the RXCLK is 25MHz,and RXER no error happen.&lt;BR /&gt;I suspect it is the configuration problem of the EB eth module. Could you please send me a EB demo project work well for S32K334 platform and TJA1101B with MII mode?&lt;/P&gt;</description>
      <pubDate>Fri, 19 Aug 2022 04:54:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-and-TJA1101B-debugging-problems/m-p/1508555#M17191</guid>
      <dc:creator>xiaomu</dc:creator>
      <dc:date>2022-08-19T04:54:49Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 and TJA1101B debugging problems</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-and-TJA1101B-debugging-problems/m-p/1511417#M17303</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Probably there were some jumper problems. You will have to move the jumper J30 on eval board from position 3-4 CLOSED to 1-2 CLOSED in order for on-board Ethernet level shifters to work properly.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Nam&lt;/P&gt;</description>
      <pubDate>Thu, 25 Aug 2022 04:29:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-and-TJA1101B-debugging-problems/m-p/1511417#M17303</guid>
      <dc:creator>namnguyenviet</dc:creator>
      <dc:date>2022-08-25T04:29:53Z</dc:date>
    </item>
  </channel>
</rss>