<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Power supply of s32K144 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Power-supply-of-s32K144/m-p/1507476#M17159</link>
    <description>&lt;P&gt;Correct,&amp;nbsp;connect the VDDA pin to the same source as VDD pin.&lt;/P&gt;</description>
    <pubDate>Wed, 17 Aug 2022 11:23:08 GMT</pubDate>
    <dc:creator>VaneB</dc:creator>
    <dc:date>2022-08-17T11:23:08Z</dc:date>
    <item>
      <title>Power supply of s32K144</title>
      <link>https://community.nxp.com/t5/S32K/Power-supply-of-s32K144/m-p/1506685#M17125</link>
      <description>&lt;P&gt;Hello Everyone,&lt;BR /&gt;&lt;BR /&gt;I was trying to explore the S32K144EVB. However, I came across a document, with the power supply layout of the board. I am attaching the screenshot of the same for your referral.&lt;BR /&gt;&lt;BR /&gt;I wanted to check if both the marked parts (VDDA) should be same or whether the left VDDA should be only from VDD. Because, I could not relate the reason of both the marked parts being the same. It doesn't make sense.&lt;BR /&gt;&lt;BR /&gt;Kindly have a look into this and help me out.&lt;BR /&gt;&lt;BR /&gt;Thank you for your time.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="s32k.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/190323iC72714611D3CCBA7/image-size/large?v=v2&amp;amp;px=999" role="button" title="s32k.png" alt="s32k.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Aug 2022 08:50:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Power-supply-of-s32K144/m-p/1506685#M17125</guid>
      <dc:creator>ankan_creatara</dc:creator>
      <dc:date>2022-08-16T08:50:40Z</dc:date>
    </item>
    <item>
      <title>Re: Power supply of s32K144</title>
      <link>https://community.nxp.com/t5/S32K/Power-supply-of-s32K144/m-p/1506807#M17130</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204712"&gt;@ankan_creatara&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;VDDA and VDD are internally connected in this package. But it has a differential of 0.1V.&lt;BR /&gt;If externally available, connect the VDDA pin to the same voltage potential as VDD.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Tue, 16 Aug 2022 12:04:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Power-supply-of-s32K144/m-p/1506807#M17130</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2022-08-16T12:04:57Z</dc:date>
    </item>
    <item>
      <title>Re: Power supply of s32K144</title>
      <link>https://community.nxp.com/t5/S32K/Power-supply-of-s32K144/m-p/1507276#M17147</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201913"&gt;@VaneB&lt;/a&gt;&amp;nbsp;,&lt;BR /&gt;&lt;BR /&gt;Thank you for your insights.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;As far as I can understand, there is no harm in connecting both the VDD and VDDA to the same source, right!!&lt;/P&gt;</description>
      <pubDate>Wed, 17 Aug 2022 07:05:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Power-supply-of-s32K144/m-p/1507276#M17147</guid>
      <dc:creator>ankan_creatara</dc:creator>
      <dc:date>2022-08-17T07:05:54Z</dc:date>
    </item>
    <item>
      <title>Re: Power supply of s32K144</title>
      <link>https://community.nxp.com/t5/S32K/Power-supply-of-s32K144/m-p/1507476#M17159</link>
      <description>&lt;P&gt;Correct,&amp;nbsp;connect the VDDA pin to the same source as VDD pin.&lt;/P&gt;</description>
      <pubDate>Wed, 17 Aug 2022 11:23:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Power-supply-of-s32K144/m-p/1507476#M17159</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2022-08-17T11:23:08Z</dc:date>
    </item>
    <item>
      <title>Re: Power supply of s32K144</title>
      <link>https://community.nxp.com/t5/S32K/Power-supply-of-s32K144/m-p/1509552#M17245</link>
      <description>&lt;P&gt;Hello Everyone,&amp;nbsp;&lt;BR /&gt;I am back with some more queries. Please help me out.&lt;BR /&gt;&lt;BR /&gt;In the overall schematic, and as far as I can understand; the S32K144EVB can be powered up in two ways:&lt;BR /&gt;1. 12V supply (external)&lt;BR /&gt;2. 5V from Micro-USB&lt;BR /&gt;&lt;BR /&gt;Please correct me if I am wrong!!&lt;BR /&gt;&lt;BR /&gt;Whenever an external 12V supply is used, the power flows through the SBC UJA1169, right? When I was exploring the UJA1169, I found out two pins in the chip:&amp;nbsp;&lt;BR /&gt;1. Pin 5: V1&lt;BR /&gt;2. Pin 14: BAT&lt;BR /&gt;&lt;BR /&gt;As I can see, V1 can be of 5V or 3.3V. Whereas BAT is the battery Voltage, which is of 5V. But, I could not find any port to connect the 12V from the external supply. Am I understanding the circuit correct? OR am I missing out something?&lt;BR /&gt;&lt;BR /&gt;Please help me in figuring out,&lt;BR /&gt;A. How can I use an external 12V supply to power up the S32K144EVB. Is it even possible to use the 12V supply or Do I need to use any 5V source?&lt;BR /&gt;B. What is the voltage at which the entire board works? Is it 12V or 5V or 3.3V?&lt;BR /&gt;&lt;BR /&gt;Thank you for your time.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Aug 2022 13:04:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Power-supply-of-s32K144/m-p/1509552#M17245</guid>
      <dc:creator>ankan_creatara</dc:creator>
      <dc:date>2022-08-22T13:04:34Z</dc:date>
    </item>
    <item>
      <title>Re: Power supply of s32K144</title>
      <link>https://community.nxp.com/t5/S32K/Power-supply-of-s32K144/m-p/1510808#M17293</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204712"&gt;@ankan_creatara&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The S32K144EVB evaluation board powers from a USB or external 12 V power supply. By default USB power is enabled with J107 jumper (2-3 closed). To enable the 12 V power you need to connect 1-2 of the J107 jumper.&lt;BR /&gt;You can refer the Datasheet and the application note AN5426:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/data-sheet/S32K-DS.pdf " target="_self"&gt;S32K-DS&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN5426 " target="_self"&gt;AN5426 &lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Wed, 24 Aug 2022 09:29:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Power-supply-of-s32K144/m-p/1510808#M17293</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2022-08-24T09:29:47Z</dc:date>
    </item>
    <item>
      <title>Re: Power supply of s32K144</title>
      <link>https://community.nxp.com/t5/S32K/Power-supply-of-s32K144/m-p/1511662#M17310</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201913"&gt;@VaneB&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thank you for your response. I will definitely look into the attached documents.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 25 Aug 2022 10:03:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Power-supply-of-s32K144/m-p/1511662#M17310</guid>
      <dc:creator>ankan_creatara</dc:creator>
      <dc:date>2022-08-25T10:03:04Z</dc:date>
    </item>
  </channel>
</rss>