<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: ADC low pass filter</title>
    <link>https://community.nxp.com/t5/S32K/ADC-low-pass-filter/m-p/1507396#M17155</link>
    <description>&lt;P&gt;Hi Bhuvana,&lt;/P&gt;
&lt;P&gt;There is no low pass filter in ADC module, you can have a look at Automatic compare function.&amp;nbsp; External hardware low pass filter can be used, but please notice the&amp;nbsp;Analog-signal source resistance(refer to &lt;A href="https://www.nxp.com/docs/en/application-note/AN4373.pdf" target="_self"&gt;AN4373 Cookbook for SAR ADC Measurements&lt;/A&gt;).&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Wed, 17 Aug 2022 09:20:01 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2022-08-17T09:20:01Z</dc:date>
    <item>
      <title>ADC low pass filter</title>
      <link>https://community.nxp.com/t5/S32K/ADC-low-pass-filter/m-p/1507305#M17150</link>
      <description>&lt;P&gt;MCU:&amp;nbsp;FS32K144UAT0VLLT&lt;BR /&gt;100LQFP&lt;/P&gt;&lt;P&gt;can we use any filter for ADC channels.&lt;/P&gt;&lt;P&gt;if there then how to enable it in software side?&lt;/P&gt;</description>
      <pubDate>Wed, 17 Aug 2022 07:35:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC-low-pass-filter/m-p/1507305#M17150</guid>
      <dc:creator>Bhuvana</dc:creator>
      <dc:date>2022-08-17T07:35:43Z</dc:date>
    </item>
    <item>
      <title>Re: ADC low pass filter</title>
      <link>https://community.nxp.com/t5/S32K/ADC-low-pass-filter/m-p/1507396#M17155</link>
      <description>&lt;P&gt;Hi Bhuvana,&lt;/P&gt;
&lt;P&gt;There is no low pass filter in ADC module, you can have a look at Automatic compare function.&amp;nbsp; External hardware low pass filter can be used, but please notice the&amp;nbsp;Analog-signal source resistance(refer to &lt;A href="https://www.nxp.com/docs/en/application-note/AN4373.pdf" target="_self"&gt;AN4373 Cookbook for SAR ADC Measurements&lt;/A&gt;).&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 17 Aug 2022 09:20:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC-low-pass-filter/m-p/1507396#M17155</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-08-17T09:20:01Z</dc:date>
    </item>
  </channel>
</rss>