<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K344 V15 from external SBC power sequence requirement in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-V15-from-external-SBC-power-sequence-requirement/m-p/1507356#M17153</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;There is an option "V15_extended defined for 1.4 - 5.5 V" in datasheet so the V15 pin can be powered also by higher voltages instead of BJT transistor regulator or 1.5V external source. So I could use 1.8V rail already available in my design to supply V15 pin while considering thermal aspects, Am I right? My goal is to save some power burned in the BJT regulator.&lt;/P&gt;&lt;P&gt;Are there any power-up, power-down sequence requirement for VDD_HV and V15 when V15 powered by external PSU or all MCU PSUs can operate independently?&lt;/P&gt;&lt;P&gt;Is there any drawback of this solution I should be aware of? I'm using 257MBGA.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How HVD_V15 set for 2.5V works if the V15_extended is defined up to 5 V? Will it trip in this case?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Karel&lt;/P&gt;</description>
    <pubDate>Wed, 17 Aug 2022 08:36:01 GMT</pubDate>
    <dc:creator>KarelAd</dc:creator>
    <dc:date>2022-08-17T08:36:01Z</dc:date>
    <item>
      <title>S32K344 V15 from external SBC power sequence requirement</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-V15-from-external-SBC-power-sequence-requirement/m-p/1507356#M17153</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;There is an option "V15_extended defined for 1.4 - 5.5 V" in datasheet so the V15 pin can be powered also by higher voltages instead of BJT transistor regulator or 1.5V external source. So I could use 1.8V rail already available in my design to supply V15 pin while considering thermal aspects, Am I right? My goal is to save some power burned in the BJT regulator.&lt;/P&gt;&lt;P&gt;Are there any power-up, power-down sequence requirement for VDD_HV and V15 when V15 powered by external PSU or all MCU PSUs can operate independently?&lt;/P&gt;&lt;P&gt;Is there any drawback of this solution I should be aware of? I'm using 257MBGA.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How HVD_V15 set for 2.5V works if the V15_extended is defined up to 5 V? Will it trip in this case?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Karel&lt;/P&gt;</description>
      <pubDate>Wed, 17 Aug 2022 08:36:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-V15-from-external-SBC-power-sequence-requirement/m-p/1507356#M17153</guid>
      <dc:creator>KarelAd</dc:creator>
      <dc:date>2022-08-17T08:36:01Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 V15 from external SBC power sequence requirement</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-V15-from-external-SBC-power-sequence-requirement/m-p/1510186#M17268</link>
      <description>&lt;P&gt;I have forwarded your question to application team, until now I don't have an answer.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Aug 2022 12:25:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-V15-from-external-SBC-power-sequence-requirement/m-p/1510186#M17268</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2022-08-23T12:25:57Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 V15 from external SBC power sequence requirement</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-V15-from-external-SBC-power-sequence-requirement/m-p/1517513#M17552</link>
      <description>&lt;P&gt;I have just obtained an answer from application team. I am sharing how it is:&lt;/P&gt;
&lt;P&gt;“From a voltage robustness perspective, just for the K31X/K32X and K34X parts allow up to 5.5V on V15.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;However&lt;/STRONG&gt;, for an application using more than 1.5V, the max die temperature Tj must be analyzed as MANDATORY. The max die temperature must not reach values beyond +150oC.&lt;/P&gt;
&lt;P&gt;It is a matter of effective thermal resistance, run current of the application and input voltage where it ends up.&lt;/P&gt;
&lt;P&gt;In my opinion, the V15_extended range is not recommendable for medium-High temperature applications.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I'm working to add these considerations and limitations in the new version of the DS”&lt;/P&gt;</description>
      <pubDate>Tue, 06 Sep 2022 08:12:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-V15-from-external-SBC-power-sequence-requirement/m-p/1517513#M17552</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2022-09-06T08:12:24Z</dc:date>
    </item>
  </channel>
</rss>