<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRAppID tool issue with K line</title>
    <link>https://community.nxp.com/t5/S32K/RAppID-tool-issue-with-K-line/m-p/722418#M1712</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello NXP team, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using S32K1XX controller in our project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have used the RappID tool for the application flashing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have downloaded rbf file from NXP forum and tried to flash the application using RappID Tool&amp;nbsp; through UART1 lines.&lt;/P&gt;&lt;P&gt;successfully flashed the application to the target board.&lt;/P&gt;&lt;P&gt;I have tried to flash the application through K line interface , application is not flashing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problem 1 :&lt;/P&gt;&lt;P&gt;&amp;nbsp;just want to know the reason , is it because of Transmission and reception is on the same line or TXINV bit not set in UART configuration in the rbf file(For K line , TXINV bit need to set in the UART configuration)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if it is the TXINV bit set , then shall we get the TXINV = 1 bit configuration rbf file?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problem 2 :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Shall we use the same rbf file for CAN and UART communication for the flashing(RAppID supports only CAN and UART interfaces)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;find the attached rbf file which we used for the application flashing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly let me know regarding this .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is high priority for us to test or flash the application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ambarish&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Mar 2018 13:41:26 GMT</pubDate>
    <dc:creator>ambarishhundeka</dc:creator>
    <dc:date>2018-03-21T13:41:26Z</dc:date>
    <item>
      <title>RAppID tool issue with K line</title>
      <link>https://community.nxp.com/t5/S32K/RAppID-tool-issue-with-K-line/m-p/722418#M1712</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello NXP team, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using S32K1XX controller in our project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have used the RappID tool for the application flashing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have downloaded rbf file from NXP forum and tried to flash the application using RappID Tool&amp;nbsp; through UART1 lines.&lt;/P&gt;&lt;P&gt;successfully flashed the application to the target board.&lt;/P&gt;&lt;P&gt;I have tried to flash the application through K line interface , application is not flashing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problem 1 :&lt;/P&gt;&lt;P&gt;&amp;nbsp;just want to know the reason , is it because of Transmission and reception is on the same line or TXINV bit not set in UART configuration in the rbf file(For K line , TXINV bit need to set in the UART configuration)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if it is the TXINV bit set , then shall we get the TXINV = 1 bit configuration rbf file?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problem 2 :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Shall we use the same rbf file for CAN and UART communication for the flashing(RAppID supports only CAN and UART interfaces)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;find the attached rbf file which we used for the application flashing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly let me know regarding this .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is high priority for us to test or flash the application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ambarish&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Mar 2018 13:41:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RAppID-tool-issue-with-K-line/m-p/722418#M1712</guid>
      <dc:creator>ambarishhundeka</dc:creator>
      <dc:date>2018-03-21T13:41:26Z</dc:date>
    </item>
  </channel>
</rss>