<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K146 watchdog timeout</title>
    <link>https://community.nxp.com/t5/S32K/S32K146-watchdog-timeout/m-p/1503832#M17002</link>
    <description>&lt;P&gt;Thank you very much for the reply, that helps a lot!&lt;/P&gt;</description>
    <pubDate>Wed, 10 Aug 2022 08:48:21 GMT</pubDate>
    <dc:creator>yqs77</dc:creator>
    <dc:date>2022-08-10T08:48:21Z</dc:date>
    <item>
      <title>S32K146 watchdog timeout</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-watchdog-timeout/m-p/1503696#M16995</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to enable a watchdog with 10 minutes timeout on S32K146, and I have noticed that&amp;nbsp;when CS[PRES] is set, the clock source is prescaled by 256 before clocking the watchdog counter which allows for longer timeout periods. But I am still wondering whether the watchdog timeout can be set to 10 minutes. If cannot, what is the maximum timeout? Thanks a lot!&lt;/P&gt;</description>
      <pubDate>Wed, 10 Aug 2022 05:50:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-watchdog-timeout/m-p/1503696#M16995</guid>
      <dc:creator>yqs77</dc:creator>
      <dc:date>2022-08-10T05:50:10Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 watchdog timeout</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-watchdog-timeout/m-p/1503756#M16997</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;WDOG has a programmable16-bit timeout counter. And the clock can be selected by&amp;nbsp;&lt;STRONG&gt;WDOG_CS[CLK]&lt;/STRONG&gt; and&amp;nbsp;&lt;STRONG&gt;SIM_LPOCLKS[LPOCLKSEL]&lt;/STRONG&gt;. If&amp;nbsp;fixed 256 clock prescaler is enabled, then it's able to achieve 10&amp;nbsp;&lt;SPAN&gt;minutes&lt;/SPAN&gt; timeout.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Table 27-9. Peripheral module clocking WDOG.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/189764i7CFBDA76A8A3241A/image-size/large?v=v2&amp;amp;px=999" role="button" title="Table 27-9. Peripheral module clocking WDOG.png" alt="Table 27-9. Peripheral module clocking WDOG.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="SIM_LPOCLKS[LPOCLKSEL].png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/189765iEBC7005BD5ED3E7C/image-size/large?v=v2&amp;amp;px=999" role="button" title="SIM_LPOCLKS[LPOCLKSEL].png" alt="SIM_LPOCLKS[LPOCLKSEL].png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 10 Aug 2022 07:16:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-watchdog-timeout/m-p/1503756#M16997</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-08-10T07:16:48Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 watchdog timeout</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-watchdog-timeout/m-p/1503832#M17002</link>
      <description>&lt;P&gt;Thank you very much for the reply, that helps a lot!&lt;/P&gt;</description>
      <pubDate>Wed, 10 Aug 2022 08:48:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-watchdog-timeout/m-p/1503832#M17002</guid>
      <dc:creator>yqs77</dc:creator>
      <dc:date>2022-08-10T08:48:21Z</dc:date>
    </item>
  </channel>
</rss>