<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Timer on S32K144 SDK</title>
    <link>https://community.nxp.com/t5/S32K/Timer-on-S32K144-SDK/m-p/1502246#M16929</link>
    <description>&lt;P&gt;I want to use timer without interrupt to wait 5s to do a job with S32K144 - SDK version on S32DS. Can you help me !&lt;/P&gt;</description>
    <pubDate>Mon, 08 Aug 2022 04:43:56 GMT</pubDate>
    <dc:creator>AnhNguyenDuc</dc:creator>
    <dc:date>2022-08-08T04:43:56Z</dc:date>
    <item>
      <title>Timer on S32K144 SDK</title>
      <link>https://community.nxp.com/t5/S32K/Timer-on-S32K144-SDK/m-p/1502246#M16929</link>
      <description>&lt;P&gt;I want to use timer without interrupt to wait 5s to do a job with S32K144 - SDK version on S32DS. Can you help me !&lt;/P&gt;</description>
      <pubDate>Mon, 08 Aug 2022 04:43:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Timer-on-S32K144-SDK/m-p/1502246#M16929</guid>
      <dc:creator>AnhNguyenDuc</dc:creator>
      <dc:date>2022-08-08T04:43:56Z</dc:date>
    </item>
    <item>
      <title>Re: Timer on S32K144 SDK</title>
      <link>https://community.nxp.com/t5/S32K/Timer-on-S32K144-SDK/m-p/1502954#M16966</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;If without interrupt how can the timer notify you the 5s is end? You may need to check the flag of that timer periodically. &lt;BR /&gt;For example:&lt;BR /&gt;LPTMR_DRV_GetCompareFlag&lt;BR /&gt;LPIT_DRV_GetInterruptFlagTimerChannels&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Have you check if the LPTMR or LPIT meet your needs? Although SDK example are with interrupt, I think you can refer to the part other than interrupt codes.&lt;/P&gt;
&lt;P&gt;SDK manual can be found here (C:\NXP\S32DS.3.4\S32DS\software\S32SDK_S32K1XX_RTM_4.0.2\doc\S32SDK_S32K144_UserManual.pdf)&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 09 Aug 2022 04:21:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Timer-on-S32K144-SDK/m-p/1502954#M16966</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-08-09T04:21:37Z</dc:date>
    </item>
  </channel>
</rss>