<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: S32K3 Wake up method</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-Wake-up-method/m-p/1501784#M16914</link>
    <description>&lt;P&gt;Hi Zhaozhang,&lt;/P&gt;
&lt;P&gt;1. No, this is not supported by LPUART. There's a note in section "76.1.1 LPUART instances and configuration":&lt;/P&gt;
&lt;P&gt;"LPUART instances are not available during Standby."&lt;/P&gt;
&lt;P&gt;2. FlexCAN itself is also not in Standby Power Domain, so you can't use the FlexCAN module directly to wake up the chip.&lt;/P&gt;
&lt;P&gt;However, there's a workaround. See the Wakeup Unit section in the reference manual. WKPU supports 4 internal sources and 60 external sources that can generate interrupts or wakeup events.&lt;BR /&gt;It also supports a non-maskable interrupt input.&lt;BR /&gt;The wakeup sources are:&lt;BR /&gt;WKPU0 : SWT0 wakeup, RTC API wakeup.&lt;BR /&gt;WKPU1 : RTC timeout.&lt;BR /&gt;WKPU2 : Round robin interrupt from any of the three comparators.&lt;BR /&gt;WKPU3 : RTI wakeup&lt;BR /&gt;WKPU4 - WKPU63 : External pin wakeup sources&lt;/P&gt;
&lt;P&gt;The external pins can be used for this purpose. LPUART_RX pins or CAN_RX pins share the function with WKPU. So, even if LPUART or FlexCAN are in low power mode, these pins can be still configured in WKPU to wake up the chip on rising or falling edge.&lt;/P&gt;
&lt;P&gt;Regards&lt;BR /&gt;Lukas&lt;/P&gt;</description>
    <pubDate>Fri, 05 Aug 2022 11:32:19 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2022-08-05T11:32:19Z</dc:date>
    <item>
      <title>S32K3 Wake up method</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-Wake-up-method/m-p/1500039#M16834</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Dear Support,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1.I see the following feature in the S32K3 RM, I wonder if this can wake up the MCU when data is received in Standby mode?&lt;/SPAN&gt;&lt;BR /&gt;Following are the features of the LPUART module.&lt;BR /&gt;Support for three receiver wakeup methods:&lt;BR /&gt;—Idle line wakeup&lt;BR /&gt;—Address mark wakeup&lt;BR /&gt;—Receive data match&lt;/P&gt;&lt;P&gt;2.&lt;SPAN&gt;S32K3 Whether the CAN RX pin CAN wake up the MCU from Standby mode after receiving data?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you for your help!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Aug 2022 07:15:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-Wake-up-method/m-p/1500039#M16834</guid>
      <dc:creator>ZhaozhangChen</dc:creator>
      <dc:date>2022-08-03T07:15:48Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 Wake up method</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-Wake-up-method/m-p/1501784#M16914</link>
      <description>&lt;P&gt;Hi Zhaozhang,&lt;/P&gt;
&lt;P&gt;1. No, this is not supported by LPUART. There's a note in section "76.1.1 LPUART instances and configuration":&lt;/P&gt;
&lt;P&gt;"LPUART instances are not available during Standby."&lt;/P&gt;
&lt;P&gt;2. FlexCAN itself is also not in Standby Power Domain, so you can't use the FlexCAN module directly to wake up the chip.&lt;/P&gt;
&lt;P&gt;However, there's a workaround. See the Wakeup Unit section in the reference manual. WKPU supports 4 internal sources and 60 external sources that can generate interrupts or wakeup events.&lt;BR /&gt;It also supports a non-maskable interrupt input.&lt;BR /&gt;The wakeup sources are:&lt;BR /&gt;WKPU0 : SWT0 wakeup, RTC API wakeup.&lt;BR /&gt;WKPU1 : RTC timeout.&lt;BR /&gt;WKPU2 : Round robin interrupt from any of the three comparators.&lt;BR /&gt;WKPU3 : RTI wakeup&lt;BR /&gt;WKPU4 - WKPU63 : External pin wakeup sources&lt;/P&gt;
&lt;P&gt;The external pins can be used for this purpose. LPUART_RX pins or CAN_RX pins share the function with WKPU. So, even if LPUART or FlexCAN are in low power mode, these pins can be still configured in WKPU to wake up the chip on rising or falling edge.&lt;/P&gt;
&lt;P&gt;Regards&lt;BR /&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 05 Aug 2022 11:32:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-Wake-up-method/m-p/1501784#M16914</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-08-05T11:32:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 Wake up method</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-Wake-up-method/m-p/1858555#M34910</link>
      <description>&lt;P&gt;We are working on s32k3112, and looking to wakeup the MCU with FlexCAN message from low power mode. Does this s32k3112 controller supports wakeup from CAN message, if yes, can you brief us how to do that ?&lt;/P&gt;&lt;P&gt;We have gone through the post, but we haven't get the clear picture. Can you elaborate on this ?&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37795"&gt;@lukaszadrapa&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/199714"&gt;@ZhaozhangChen&lt;/a&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 02 May 2024 18:28:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-Wake-up-method/m-p/1858555#M34910</guid>
      <dc:creator>dheeraj</dc:creator>
      <dc:date>2024-05-02T18:28:09Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 Wake up method</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-Wake-up-method/m-p/1891395#M36784</link>
      <description>&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;I am working on sleep mode and wake up mode on S32k324 controller.&lt;/P&gt;&lt;P&gt;Can you plz share me the sample code for sleep and wake up from GPIO and can&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jun 2024 12:00:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-Wake-up-method/m-p/1891395#M36784</guid>
      <dc:creator>Prasad_330</dc:creator>
      <dc:date>2024-06-20T12:00:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 Wake up method</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-Wake-up-method/m-p/2297418#M56253</link>
      <description>&lt;P&gt;I am new to the S32Kxx microcontroller and AUTOSAR, and I’m using EB tresos for MCAL configuration. My goal is to transition the system from RUN mode to STANDBY, and then wake it up back to RUN mode when an external pin (the ignition pin) is activated. I want to configure this pin as a wakeup interrupt source.&lt;/P&gt;&lt;P&gt;If anyone has experience with similar use cases, I would greatly appreciate your guidance. Even a basic sample code or configuration steps to get started would be very helpful. Thank you!&lt;BR /&gt;I'm using s32k314 series.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jan 2026 13:13:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-Wake-up-method/m-p/2297418#M56253</guid>
      <dc:creator>mithun_ccc</dc:creator>
      <dc:date>2026-01-21T13:13:59Z</dc:date>
    </item>
  </channel>
</rss>