<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 S32144-LOC</title>
    <link>https://community.nxp.com/t5/S32K/S32144-LOC/m-p/1501117#M16889</link>
    <description>&lt;P&gt;May I ask if the S32K144 software does not operate properly and triggers SOSCERR to be set when the SOSC clock monitor is turned on? I tried entering (all) low power modes after turning on the clock monitor, and I can see that SOSC becomes invalid (SOSCVLD=0) but no SOSCERR is generated.&lt;/P&gt;</description>
    <pubDate>Thu, 04 Aug 2022 12:16:36 GMT</pubDate>
    <dc:creator>Junkie</dc:creator>
    <dc:date>2022-08-04T12:16:36Z</dc:date>
    <item>
      <title>S32144-LOC</title>
      <link>https://community.nxp.com/t5/S32K/S32144-LOC/m-p/1501117#M16889</link>
      <description>&lt;P&gt;May I ask if the S32K144 software does not operate properly and triggers SOSCERR to be set when the SOSC clock monitor is turned on? I tried entering (all) low power modes after turning on the clock monitor, and I can see that SOSC becomes invalid (SOSCVLD=0) but no SOSCERR is generated.&lt;/P&gt;</description>
      <pubDate>Thu, 04 Aug 2022 12:16:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32144-LOC/m-p/1501117#M16889</guid>
      <dc:creator>Junkie</dc:creator>
      <dc:date>2022-08-04T12:16:36Z</dc:date>
    </item>
    <item>
      <title>Re: S32144-LOC</title>
      <link>https://community.nxp.com/t5/S32K/S32144-LOC/m-p/1503114#M16970</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I'm not sure if I can understand the question but clock monitors should not be used in low power modes:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lukaszadrapa_0-1660033659856.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/189619i05770A39A68DB9BA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lukaszadrapa_0-1660033659856.png" alt="lukaszadrapa_0-1660033659856.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Tue, 09 Aug 2022 08:27:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32144-LOC/m-p/1503114#M16970</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-08-09T08:27:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32144-LOC</title>
      <link>https://community.nxp.com/t5/S32K/S32144-LOC/m-p/1503176#M16972</link>
      <description>&lt;P&gt;Yes, it is mentioned in the reference manual that SOSC monitor cannot be used in low power mode. But my purpose is to cause a LOC error to reset the MCU, I caused the LOC error by shorting the external SOSC crystal to ground, but is there a way to use software? I've tried going into low power mode to cause the LOC error but it doesn't work.&lt;/P&gt;</description>
      <pubDate>Tue, 09 Aug 2022 09:25:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32144-LOC/m-p/1503176#M16972</guid>
      <dc:creator>Junkie</dc:creator>
      <dc:date>2022-08-09T09:25:37Z</dc:date>
    </item>
    <item>
      <title>Re: S32144-LOC</title>
      <link>https://community.nxp.com/t5/S32K/S32144-LOC/m-p/1503931#M17010</link>
      <description>&lt;P&gt;Well, I can't see simple way how to inject this error by software. As you mentioned, for test purposes such error is usually injected by shorting of OSC circuit in hardware.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Wed, 10 Aug 2022 11:03:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32144-LOC/m-p/1503931#M17010</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-08-10T11:03:04Z</dc:date>
    </item>
    <item>
      <title>Re: S32144-LOC</title>
      <link>https://community.nxp.com/t5/S32K/S32144-LOC/m-p/1541924#M18474</link>
      <description>OK, thank you very much.</description>
      <pubDate>Fri, 21 Oct 2022 10:13:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32144-LOC/m-p/1541924#M18474</guid>
      <dc:creator>Junkie</dc:creator>
      <dc:date>2022-10-21T10:13:49Z</dc:date>
    </item>
  </channel>
</rss>