<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Temperature detection function in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Temperature-detection-function/m-p/1500322#M16853</link>
    <description>&lt;P&gt;Hi&amp;nbsp;JackChen2022,&lt;/P&gt;
&lt;P&gt;Please refer to:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/S32K148-ADC-Temp-Sense/m-p/1071115" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K148-ADC-Temp-Sense/m-p/1071115&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Wed, 03 Aug 2022 13:56:49 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2022-08-03T13:56:49Z</dc:date>
    <item>
      <title>Temperature detection function</title>
      <link>https://community.nxp.com/t5/S32K/Temperature-detection-function/m-p/1499972#M16833</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello, I would like to know if the S32K14* series chips have a temperature detection function, or if the entire S32K series has this function, you can also provide reference.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Aug 2022 05:22:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Temperature-detection-function/m-p/1499972#M16833</guid>
      <dc:creator>JackChen2022</dc:creator>
      <dc:date>2022-08-03T05:22:00Z</dc:date>
    </item>
    <item>
      <title>Re: Temperature detection function</title>
      <link>https://community.nxp.com/t5/S32K/Temperature-detection-function/m-p/1500322#M16853</link>
      <description>&lt;P&gt;Hi&amp;nbsp;JackChen2022,&lt;/P&gt;
&lt;P&gt;Please refer to:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/S32K148-ADC-Temp-Sense/m-p/1071115" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K148-ADC-Temp-Sense/m-p/1071115&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 03 Aug 2022 13:56:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Temperature-detection-function/m-p/1500322#M16853</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-08-03T13:56:49Z</dc:date>
    </item>
    <item>
      <title>Re: Temperature detection function</title>
      <link>https://community.nxp.com/t5/S32K/Temperature-detection-function/m-p/1501041#M16887</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Hi&amp;nbsp;&lt;SPAN class=""&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/57959" target="_self"&gt;&lt;SPAN class=""&gt;Robin_Shen&lt;/SPAN&gt;&lt;/A&gt;&amp;nbsp;,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;After reading your reply, I understand that the function of the internal temperature sensor may be supported on earlier hardware, and the existing version may be removed?&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;At the same time, some sample programs are not available yet, right?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Aug 2022 10:20:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Temperature-detection-function/m-p/1501041#M16887</guid>
      <dc:creator>JackChen2022</dc:creator>
      <dc:date>2022-08-04T10:20:26Z</dc:date>
    </item>
    <item>
      <title>Re: Temperature detection function</title>
      <link>https://community.nxp.com/t5/S32K/Temperature-detection-function/m-p/1501146#M16890</link>
      <description>&lt;P&gt;&lt;SPAN&gt;&lt;EM&gt;the existing version may be removed?&lt;/EM&gt; no&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;EM&gt;some sample programs are not available yet, right?&lt;/EM&gt; still not sample programs.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Aug 2022 13:03:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Temperature-detection-function/m-p/1501146#M16890</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-08-04T13:03:18Z</dc:date>
    </item>
  </channel>
</rss>