<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K146 CAN callback function will only enter once in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K146-CAN-callback-function-will-only-enter-once/m-p/1497268#M16714</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;after callback is called you need to call&amp;nbsp;CAN_Receive to start&amp;nbsp;receiving data in given RX MB again.&lt;BR /&gt;Can be done in callback, i think, after you process data.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Thu, 28 Jul 2022 10:44:53 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2022-07-28T10:44:53Z</dc:date>
    <item>
      <title>S32K146 CAN callback function will only enter once</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-CAN-callback-function-will-only-enter-once/m-p/1496152#M16678</link>
      <description>&lt;P&gt;Hello EveryOne,&lt;/P&gt;&lt;P&gt;Init can_pal module and test can function, I find can tx function is ok, but CAN callback function will only enter once, if continue send can message from tester, system will not enter callback function.&lt;/P&gt;&lt;P&gt;The detail information refer to the attachment.&lt;/P&gt;&lt;P&gt;thanks!&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="547416104_0-1658906363860.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/188002iDA353BA71CB840E9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="547416104_0-1658906363860.png" alt="547416104_0-1658906363860.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jul 2022 07:19:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-CAN-callback-function-will-only-enter-once/m-p/1496152#M16678</guid>
      <dc:creator>547416104</dc:creator>
      <dc:date>2022-07-27T07:19:35Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 CAN callback function will only enter once</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-CAN-callback-function-will-only-enter-once/m-p/1497268#M16714</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;after callback is called you need to call&amp;nbsp;CAN_Receive to start&amp;nbsp;receiving data in given RX MB again.&lt;BR /&gt;Can be done in callback, i think, after you process data.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 28 Jul 2022 10:44:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-CAN-callback-function-will-only-enter-once/m-p/1497268#M16714</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-07-28T10:44:53Z</dc:date>
    </item>
  </channel>
</rss>