<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Query about Disabling Lockstep core in S32K344 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Query-about-Disabling-Lockstep-core-in-S32K344/m-p/1496344#M16686</link>
    <description>&lt;P&gt;1) Yes, if you program new DCF client with LOCKSTEP_EN = 0, it makes checker core as independent.&lt;/P&gt;
&lt;P&gt;2) Yes, it’ll behave as second core connected over separate XBAR port.&lt;/P&gt;
&lt;P&gt;Programming of DCF records is not trivial task but it is manageable. User would be aware that he can easily destroy the chip in case the programming is not done properly and the device may never exit from reset. It is simpler to order S32K324 that have decoupled cores by default, in other aspect it is the same.&lt;/P&gt;</description>
    <pubDate>Wed, 27 Jul 2022 11:46:15 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2022-07-27T11:46:15Z</dc:date>
    <item>
      <title>Query about Disabling Lockstep core in S32K344</title>
      <link>https://community.nxp.com/t5/S32K/Query-about-Disabling-Lockstep-core-in-S32K344/m-p/1494539#M16606</link>
      <description>&lt;P&gt;As per user guide to S32K3 Disable lockstep , if we disable lockstep CPU core using DCF records&lt;BR /&gt;1. Are we able to use Checker core as an independent core?&lt;BR /&gt;2. In terms of functionality &amp;amp; Performance , will it behave as master core?&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jul 2022 06:31:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Query-about-Disabling-Lockstep-core-in-S32K344/m-p/1494539#M16606</guid>
      <dc:creator>Dharanidharan_S</dc:creator>
      <dc:date>2022-07-25T06:31:17Z</dc:date>
    </item>
    <item>
      <title>Re: Query about Disabling Lockstep core in S32K344</title>
      <link>https://community.nxp.com/t5/S32K/Query-about-Disabling-Lockstep-core-in-S32K344/m-p/1496344#M16686</link>
      <description>&lt;P&gt;1) Yes, if you program new DCF client with LOCKSTEP_EN = 0, it makes checker core as independent.&lt;/P&gt;
&lt;P&gt;2) Yes, it’ll behave as second core connected over separate XBAR port.&lt;/P&gt;
&lt;P&gt;Programming of DCF records is not trivial task but it is manageable. User would be aware that he can easily destroy the chip in case the programming is not done properly and the device may never exit from reset. It is simpler to order S32K324 that have decoupled cores by default, in other aspect it is the same.&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jul 2022 11:46:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Query-about-Disabling-Lockstep-core-in-S32K344/m-p/1496344#M16686</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2022-07-27T11:46:15Z</dc:date>
    </item>
  </channel>
</rss>