<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Wake-up from VLPS in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Wake-up-from-VLPS/m-p/720050#M1653</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Finally, I found the issue. Actually, the MCU was never gone to VLPS. Instead watchdog was enabled in stop mode what is causing problems and cut supply. It is is normal that after that the MCU could not be waked up. When disabling watchdog in stop mode, every thing is working well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 Nov 2017 13:19:21 GMT</pubDate>
    <dc:creator>youssef</dc:creator>
    <dc:date>2017-11-20T13:19:21Z</dc:date>
    <item>
      <title>Wake-up from VLPS</title>
      <link>https://community.nxp.com/t5/S32K/Wake-up-from-VLPS/m-p/720049#M1652</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once entering in VLPS mode,&amp;nbsp;an interrupt&amp;nbsp;external input can not wake up MCU.&lt;/P&gt;&lt;P&gt;The PTC12 is configured as GPIO input and rising edge interrupt is enabled on it.&lt;/P&gt;&lt;P&gt;I configure an interrupt handler to just clear the ISF bit.&lt;/P&gt;&lt;P&gt;I use this code to enter in VLPS:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SMC-&amp;gt;PMPROT |= SMC_PMPROT_AVLP(1);&lt;BR /&gt; /* Select VLPS mode */&lt;BR /&gt; SMC-&amp;gt;PMCTRL = SMC_PMCTRL_STOPM(0b010);&lt;BR /&gt; /*wait for write to complete to SMC before stopping core */&lt;BR /&gt; dummyread = SMC-&amp;gt;PMCTRL;&lt;BR /&gt; dummyread++;&lt;BR /&gt; /* Enable SLEEPDEEP bit in the core */&lt;BR /&gt; S32_SCB-&amp;gt;SCR |= S32_SCB_SCR_SLEEPDEEP_MASK;&lt;BR /&gt; /* Waiting for next interrupt will get micro in sleep mode */&lt;BR /&gt; STANDBY();&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The GPIO interrupt is tested and working correctelly before the MCU goes to VLPS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So why can not wake up from VLPS? M I missing something?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Youssef&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Nov 2017 18:29:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Wake-up-from-VLPS/m-p/720049#M1652</guid>
      <dc:creator>youssef</dc:creator>
      <dc:date>2017-11-17T18:29:01Z</dc:date>
    </item>
    <item>
      <title>Re: Wake-up from VLPS</title>
      <link>https://community.nxp.com/t5/S32K/Wake-up-from-VLPS/m-p/720050#M1653</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Finally, I found the issue. Actually, the MCU was never gone to VLPS. Instead watchdog was enabled in stop mode what is causing problems and cut supply. It is is normal that after that the MCU could not be waked up. When disabling watchdog in stop mode, every thing is working well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Nov 2017 13:19:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Wake-up-from-VLPS/m-p/720050#M1653</guid>
      <dc:creator>youssef</dc:creator>
      <dc:date>2017-11-20T13:19:21Z</dc:date>
    </item>
  </channel>
</rss>