<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックOutput voltaje thersholds versus Source Current</title>
    <link>https://community.nxp.com/t5/S32K/Output-voltaje-thersholds-versus-Source-Current/m-p/1490530#M16405</link>
    <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I need to know the logical digital output thresholds of the S32K1xx series, based on the current supplied for the range of VDD = 3.3V.&lt;/P&gt;&lt;P&gt;Already consulted the Table 17- Datasheet (S32K-DS) but they are only specified for certain currents (3mA-3.5mA to VDD = 3.3V) , as well as the Figure 8 - AN2434 that only specifies it for VDD = 5V.&lt;/P&gt;</description>
    <pubDate>Fri, 15 Jul 2022 22:14:57 GMT</pubDate>
    <dc:creator>DiegoRC</dc:creator>
    <dc:date>2022-07-15T22:14:57Z</dc:date>
    <item>
      <title>Output voltaje thersholds versus Source Current</title>
      <link>https://community.nxp.com/t5/S32K/Output-voltaje-thersholds-versus-Source-Current/m-p/1490530#M16405</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I need to know the logical digital output thresholds of the S32K1xx series, based on the current supplied for the range of VDD = 3.3V.&lt;/P&gt;&lt;P&gt;Already consulted the Table 17- Datasheet (S32K-DS) but they are only specified for certain currents (3mA-3.5mA to VDD = 3.3V) , as well as the Figure 8 - AN2434 that only specifies it for VDD = 5V.&lt;/P&gt;</description>
      <pubDate>Fri, 15 Jul 2022 22:14:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Output-voltaje-thersholds-versus-Source-Current/m-p/1490530#M16405</guid>
      <dc:creator>DiegoRC</dc:creator>
      <dc:date>2022-07-15T22:14:57Z</dc:date>
    </item>
    <item>
      <title>Re: Output voltaje thersholds versus Source Current</title>
      <link>https://community.nxp.com/t5/S32K/Output-voltaje-thersholds-versus-Source-Current/m-p/1491086#M16459</link>
      <description>&lt;P&gt;Specified Voh/Vol is min/max value when sourcing/sinking current is Ioh/Iol as specified.&lt;BR /&gt;V-I characteristic for logic 1 (output) can estimated by linear approximation between points and &amp;lt;Ioh;Voh&amp;gt; and &amp;lt;0mA ; VDD&amp;gt;. The same way you can estimate V-I characteristic for logic 0.&lt;/P&gt;</description>
      <pubDate>Mon, 18 Jul 2022 13:42:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Output-voltaje-thersholds-versus-Source-Current/m-p/1491086#M16459</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2022-07-18T13:42:36Z</dc:date>
    </item>
    <item>
      <title>Re: Output voltaje thersholds versus Source Current</title>
      <link>https://community.nxp.com/t5/S32K/Output-voltaje-thersholds-versus-Source-Current/m-p/1491248#M16463</link>
      <description>&lt;P&gt;Hello. Thanks for the support.&lt;/P&gt;&lt;P&gt;For an estimate it seems valid to me. But not for a "worst-case analysis" (as is my case).&lt;/P&gt;&lt;P&gt;Is it the only theoretical way to get the thresholds?&lt;/P&gt;&lt;P&gt;Is there no such data?&lt;/P&gt;</description>
      <pubDate>Mon, 18 Jul 2022 19:44:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Output-voltaje-thersholds-versus-Source-Current/m-p/1491248#M16463</guid>
      <dc:creator>DiegoRC</dc:creator>
      <dc:date>2022-07-18T19:44:51Z</dc:date>
    </item>
    <item>
      <title>Re: Output voltaje thersholds versus Source Current</title>
      <link>https://community.nxp.com/t5/S32K/Output-voltaje-thersholds-versus-Source-Current/m-p/1492426#M16521</link>
      <description>&lt;P&gt;How it is defined (i.e. minimum current at defined voltage) it is basically worst case.&lt;/P&gt;
&lt;P&gt;You can also use IBIS model we are providing.&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jul 2022 11:35:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Output-voltaje-thersholds-versus-Source-Current/m-p/1492426#M16521</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2022-07-20T11:35:45Z</dc:date>
    </item>
    <item>
      <title>Re: Output voltaje thersholds versus Source Current</title>
      <link>https://community.nxp.com/t5/S32K/Output-voltaje-thersholds-versus-Source-Current/m-p/2161674#M52311</link>
      <description>&lt;P&gt;Hi David：&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Does the S32K1 have the threshold data for VOL and VOH? If it depends on the sourcing/sinking current? Can VOL_max be calculated through the formula of MOS transistor's resistance * sink maximum current? Can we obtain this data?&lt;/P&gt;</description>
      <pubDate>Tue, 02 Sep 2025 02:09:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Output-voltaje-thersholds-versus-Source-Current/m-p/2161674#M52311</guid>
      <dc:creator>seanli_study</dc:creator>
      <dc:date>2025-09-02T02:09:26Z</dc:date>
    </item>
  </channel>
</rss>