<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K146 GPIO port has no function when lpit module is running in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K146-GPIO-port-has-no-function-when-lpit-module-is-running/m-p/1488402#M16324</link>
    <description>&lt;P&gt;&lt;A href="mailto:Hi@547416104" target="_blank"&gt;Hi@547416104&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hi, can you send me your project, i need to double check it.&lt;/P&gt;</description>
    <pubDate>Wed, 13 Jul 2022 02:29:14 GMT</pubDate>
    <dc:creator>Senlent</dc:creator>
    <dc:date>2022-07-13T02:29:14Z</dc:date>
    <item>
      <title>S32K146 GPIO port has no function when lpit module is running</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-GPIO-port-has-no-function-when-lpit-module-is-running/m-p/1488199#M16320</link>
      <description>&lt;P&gt;Hello EveryOne,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I found the GPIO ports have no function when enable the lpit module, then I can not detect the gpio port power level changed and can output power level via gpio output port.&lt;/P&gt;&lt;P&gt;If disable the lpit module, the the gpio ports are work normal.&lt;/P&gt;&lt;P&gt;the code as the follow picture:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="547416104_0-1657636215827.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/186348i9A6149094EB6C8DF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="547416104_0-1657636215827.png" alt="547416104_0-1657636215827.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jul 2022 14:30:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-GPIO-port-has-no-function-when-lpit-module-is-running/m-p/1488199#M16320</guid>
      <dc:creator>547416104</dc:creator>
      <dc:date>2022-07-12T14:30:43Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 GPIO port has no function when lpit module is running</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-GPIO-port-has-no-function-when-lpit-module-is-running/m-p/1488402#M16324</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@547416104" target="_blank"&gt;Hi@547416104&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hi, can you send me your project, i need to double check it.&lt;/P&gt;</description>
      <pubDate>Wed, 13 Jul 2022 02:29:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-GPIO-port-has-no-function-when-lpit-module-is-running/m-p/1488402#M16324</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2022-07-13T02:29:14Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 GPIO port has no function when lpit module is running</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-GPIO-port-has-no-function-when-lpit-module-is-running/m-p/1488407#M16325</link>
      <description>&lt;P&gt;Hello Senlent,&lt;/P&gt;&lt;P&gt;I have attached the demo project, please check the attachment for detail. if you have any questions, please told me, thanks a lot.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Jul 2022 02:39:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-GPIO-port-has-no-function-when-lpit-module-is-running/m-p/1488407#M16325</guid>
      <dc:creator>547416104</dc:creator>
      <dc:date>2022-07-13T02:39:30Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 GPIO port has no function when lpit module is running</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-GPIO-port-has-no-function-when-lpit-module-is-running/m-p/1488428#M16326</link>
      <description>&lt;P&gt;I did't find any code related to this question.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_0-1657682253514.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/186395i22F406CD1009E96E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Senlent_0-1657682253514.png" alt="Senlent_0-1657682253514.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Jul 2022 03:18:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-GPIO-port-has-no-function-when-lpit-module-is-running/m-p/1488428#M16326</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2022-07-13T03:18:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 GPIO port has no function when lpit module is running</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-GPIO-port-has-no-function-when-lpit-module-is-running/m-p/1488532#M16329</link>
      <description>&lt;P&gt;I'm very sorry, please refer to the follow attachment, thanks&lt;/P&gt;</description>
      <pubDate>Wed, 13 Jul 2022 06:40:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-GPIO-port-has-no-function-when-lpit-module-is-running/m-p/1488532#M16329</guid>
      <dc:creator>547416104</dc:creator>
      <dc:date>2022-07-13T06:40:36Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 GPIO port has no function when lpit module is running</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-GPIO-port-has-no-function-when-lpit-module-is-running/m-p/1488648#M16333</link>
      <description>&lt;P&gt;Hello Senlent,&lt;/P&gt;&lt;P&gt;I have fixed the problem, the root cause is configure mistake, I updated the configure, the gpio module and lpit module are all ok.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Jul 2022 09:18:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-GPIO-port-has-no-function-when-lpit-module-is-running/m-p/1488648#M16333</guid>
      <dc:creator>547416104</dc:creator>
      <dc:date>2022-07-13T09:18:44Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 GPIO port has no function when lpit module is running</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-GPIO-port-has-no-function-when-lpit-module-is-running/m-p/1488659#M16334</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@547416104" target="_blank"&gt;Hi@547416104&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;you set the timer period to 1 prevent the PC from&amp;nbsp; jumping to main-loop.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_0-1657703159510.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/186435i800BBD60A4013F49/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Senlent_0-1657703159510.png" alt="Senlent_0-1657703159510.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Jul 2022 09:26:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-GPIO-port-has-no-function-when-lpit-module-is-running/m-p/1488659#M16334</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2022-07-13T09:26:31Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 GPIO port has no function when lpit module is running</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-GPIO-port-has-no-function-when-lpit-module-is-running/m-p/1488810#M16341</link>
      <description>&lt;P&gt;Yes，you are right, I just updated the item, thanks a lot!&lt;/P&gt;</description>
      <pubDate>Wed, 13 Jul 2022 13:41:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-GPIO-port-has-no-function-when-lpit-module-is-running/m-p/1488810#M16341</guid>
      <dc:creator>547416104</dc:creator>
      <dc:date>2022-07-13T13:41:38Z</dc:date>
    </item>
  </channel>
</rss>