<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K ADC transfer function in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K-ADC-transfer-function/m-p/1484475#M16208</link>
    <description>&lt;P&gt;First of all sorry for the late reply (project priorities currently have changed).&lt;/P&gt;&lt;P&gt;I'll try to give an example:&lt;/P&gt;&lt;P&gt;Would I read (in an ideal world) a 1 from the result register if the analog input's voltage reaches&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;0.5 LBS&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;or only if it reaches&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;1 LSB?&lt;/LI&gt;&lt;/UL&gt;</description>
    <pubDate>Tue, 05 Jul 2022 09:50:47 GMT</pubDate>
    <dc:creator>muellermathias</dc:creator>
    <dc:date>2022-07-05T09:50:47Z</dc:date>
    <item>
      <title>S32K ADC transfer function</title>
      <link>https://community.nxp.com/t5/S32K/S32K-ADC-transfer-function/m-p/1474255#M15940</link>
      <description>&lt;P&gt;In the application note AN12217 two different ADC transfer functions are presented:&lt;A href="https://www.nxp.com/docs/en/application-note/AN12217.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12217.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="adc_transfer_function.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/183439i704940A0040A13BD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="adc_transfer_function.png" alt="adc_transfer_function.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;adc_transfer_function.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Unfortunately I could not find any information _which_ is actually implemented in the S32k controllers (in our case S32K144).&lt;/P&gt;&lt;P&gt;Are you able to provide this information?&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jun 2022 08:06:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-ADC-transfer-function/m-p/1474255#M15940</guid>
      <dc:creator>muellermathias</dc:creator>
      <dc:date>2022-06-15T08:06:07Z</dc:date>
    </item>
    <item>
      <title>Re: S32K ADC transfer function</title>
      <link>https://community.nxp.com/t5/S32K/S32K-ADC-transfer-function/m-p/1474878#M15954</link>
      <description>&lt;P&gt;Hi&amp;nbsp;muellermathias,&lt;/P&gt;
&lt;P&gt;Sorry. We did not offer ADC &lt;STRONG&gt;Actual&lt;/STRONG&gt; Transfer Function.(You can &lt;STRONG&gt;not&lt;/STRONG&gt; find the curve describing this behavior is the actual transfer function and includes all the errors inherent to the ADC module itself.)&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="AN12217 ADC Actual Transfer Function.png" style="width: 885px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/183531i9C928A5354797E17/image-size/large?v=v2&amp;amp;px=999" role="button" title="AN12217 ADC Actual Transfer Function.png" alt="AN12217 ADC Actual Transfer Function.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;AN12217 ADC Actual Transfer Function.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;The following ADC specifications can be known from &lt;A href="https://www.nxp.com/docs/en/data-sheet/S32K-DS.pdf" target="_self"&gt;S32K1xx MCU Family - Data Sheet&lt;/A&gt;:&lt;BR /&gt;Differential Non-Linearity (DNL)&lt;BR /&gt;Integral Non-Linearity(INL)&lt;BR /&gt;Total Unadjusted Error (TUE)&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jun 2022 01:02:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-ADC-transfer-function/m-p/1474878#M15954</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-06-16T01:02:04Z</dc:date>
    </item>
    <item>
      <title>Re: S32K ADC transfer function</title>
      <link>https://community.nxp.com/t5/S32K/S32K-ADC-transfer-function/m-p/1478834#M16041</link>
      <description>&lt;P&gt;Hello Robin,&lt;/P&gt;&lt;P&gt;I realize that the ideal transfer function cannot be represented by the actual hardware, but surely there must have been a design goal which type of transfer function should be implemented (compensated or uncompensated)?&lt;/P&gt;&lt;P&gt;But maybe I still have an understanding problem there...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mathias&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jun 2022 07:44:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-ADC-transfer-function/m-p/1478834#M16041</guid>
      <dc:creator>muellermathias</dc:creator>
      <dc:date>2022-06-23T07:44:34Z</dc:date>
    </item>
    <item>
      <title>Re: S32K ADC transfer function</title>
      <link>https://community.nxp.com/t5/S32K/S32K-ADC-transfer-function/m-p/1483973#M16181</link>
      <description>&lt;P&gt;Hi Mathias,&lt;/P&gt;
&lt;P&gt;I'm not sure if I understand what you need, can you show me an example.&amp;nbsp;For the case of 12-bit ADC reference voltage of 5V, does ideal transfer function mean:&amp;nbsp;&lt;SPAN&gt;result=4096*Vin/5 ?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;BR /&gt;Robin&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 04 Jul 2022 09:31:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-ADC-transfer-function/m-p/1483973#M16181</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-07-04T09:31:45Z</dc:date>
    </item>
    <item>
      <title>Re: S32K ADC transfer function</title>
      <link>https://community.nxp.com/t5/S32K/S32K-ADC-transfer-function/m-p/1484475#M16208</link>
      <description>&lt;P&gt;First of all sorry for the late reply (project priorities currently have changed).&lt;/P&gt;&lt;P&gt;I'll try to give an example:&lt;/P&gt;&lt;P&gt;Would I read (in an ideal world) a 1 from the result register if the analog input's voltage reaches&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;0.5 LBS&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;or only if it reaches&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;1 LSB?&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Tue, 05 Jul 2022 09:50:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-ADC-transfer-function/m-p/1484475#M16208</guid>
      <dc:creator>muellermathias</dc:creator>
      <dc:date>2022-07-05T09:50:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32K ADC transfer function</title>
      <link>https://community.nxp.com/t5/S32K/S32K-ADC-transfer-function/m-p/1484973#M16218</link>
      <description>&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5250.pdf" target="_self"&gt;AN5250&lt;/A&gt; How to Increase the Analog-to-Digital Converter Accuracy in an Application&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="3.1.1. Offset error.png" style="width: 689px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/185667iBAC28572202A67DD/image-size/large?v=v2&amp;amp;px=999" role="button" title="3.1.1. Offset error.png" alt="3.1.1. Offset error.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;3.1.1. Offset error.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Jul 2022 02:22:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-ADC-transfer-function/m-p/1484973#M16218</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-07-06T02:22:12Z</dc:date>
    </item>
  </channel>
</rss>