<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックADC Safety Test</title>
    <link>https://community.nxp.com/t5/S32K/ADC-Safety-Test/m-p/1482663#M16150</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to test adc for safety mechanism. There is an expression in the document like this :&lt;/P&gt;&lt;P&gt;"Enable and configure the ADC internal supply monitoring feature to sample and convert the fixed internal voltages of 0 V and 5 V. Then, compare the conversion results with the corresponding expected values."&lt;/P&gt;&lt;P&gt;" configure the ADC to convert two fixed internal constant values, followed by an application-dependent voltage value. Then, compare the conversion results with the expected values. Choose an application-dependent voltage value that is between the two fixed constant values. Perform a conversion in both directions -- from low voltage to high voltage, and from high voltage to low voltage."&lt;/P&gt;&lt;P&gt;I dont understand how can I read 0V and how can I control these test runtime?&lt;/P&gt;</description>
    <pubDate>Wed, 03 Aug 2022 09:40:45 GMT</pubDate>
    <dc:creator>smt87</dc:creator>
    <dc:date>2022-08-03T09:40:45Z</dc:date>
    <item>
      <title>ADC Safety Test</title>
      <link>https://community.nxp.com/t5/S32K/ADC-Safety-Test/m-p/1482663#M16150</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to test adc for safety mechanism. There is an expression in the document like this :&lt;/P&gt;&lt;P&gt;"Enable and configure the ADC internal supply monitoring feature to sample and convert the fixed internal voltages of 0 V and 5 V. Then, compare the conversion results with the corresponding expected values."&lt;/P&gt;&lt;P&gt;" configure the ADC to convert two fixed internal constant values, followed by an application-dependent voltage value. Then, compare the conversion results with the expected values. Choose an application-dependent voltage value that is between the two fixed constant values. Perform a conversion in both directions -- from low voltage to high voltage, and from high voltage to low voltage."&lt;/P&gt;&lt;P&gt;I dont understand how can I read 0V and how can I control these test runtime?&lt;/P&gt;</description>
      <pubDate>Wed, 03 Aug 2022 09:40:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC-Safety-Test/m-p/1482663#M16150</guid>
      <dc:creator>smt87</dc:creator>
      <dc:date>2022-08-03T09:40:45Z</dc:date>
    </item>
  </channel>
</rss>