<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックCAN-FD communication fail using  TJA1145FD</title>
    <link>https://community.nxp.com/t5/S32K/CAN-FD-communication-fail-using-TJA1145FD/m-p/1477346#M16012</link>
    <description>&lt;P&gt;Hello, NXP support,&lt;/P&gt;&lt;P&gt;Now I am debugging CAN-FD&amp;amp;TJA1145FD using s32k144. The phenomenon is as follows.&lt;BR /&gt;S32K144 + CAN-FD + TJA1043&lt;BR /&gt;→CAN-FD communication(send/receive) is &lt;SPAN&gt;successful&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;S32K144 + CAN + TJA1145FD&lt;BR /&gt;→CAN communication(send/receive) is &lt;SPAN&gt;successful&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;S32K144 + CAN-FD + TJA1145FD&lt;BR /&gt;→CAN communication fails.&lt;BR /&gt;→PC CAN Box Tool displays “error frame" in output window.&lt;BR /&gt;→TJA1145FD 's TX pin has waveform, but it is different from the waveform of CAN-FD&amp;amp;TJA1043.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&amp;lt;Question&amp;gt;&lt;BR /&gt;Why does the communication fail when MCU uses CAN-FD&amp;amp;TJA1145FD ?&lt;BR /&gt;Is there any difference in the control method or configuration method of TJA1145FD when MCU uses CAN and CAN-FD?&lt;/P&gt;&lt;P&gt;With Best Regards,&lt;/P&gt;</description>
    <pubDate>Tue, 21 Jun 2022 09:34:50 GMT</pubDate>
    <dc:creator>chengsz12060</dc:creator>
    <dc:date>2022-06-21T09:34:50Z</dc:date>
    <item>
      <title>CAN-FD communication fail using  TJA1145FD</title>
      <link>https://community.nxp.com/t5/S32K/CAN-FD-communication-fail-using-TJA1145FD/m-p/1477346#M16012</link>
      <description>&lt;P&gt;Hello, NXP support,&lt;/P&gt;&lt;P&gt;Now I am debugging CAN-FD&amp;amp;TJA1145FD using s32k144. The phenomenon is as follows.&lt;BR /&gt;S32K144 + CAN-FD + TJA1043&lt;BR /&gt;→CAN-FD communication(send/receive) is &lt;SPAN&gt;successful&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;S32K144 + CAN + TJA1145FD&lt;BR /&gt;→CAN communication(send/receive) is &lt;SPAN&gt;successful&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;S32K144 + CAN-FD + TJA1145FD&lt;BR /&gt;→CAN communication fails.&lt;BR /&gt;→PC CAN Box Tool displays “error frame" in output window.&lt;BR /&gt;→TJA1145FD 's TX pin has waveform, but it is different from the waveform of CAN-FD&amp;amp;TJA1043.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&amp;lt;Question&amp;gt;&lt;BR /&gt;Why does the communication fail when MCU uses CAN-FD&amp;amp;TJA1145FD ?&lt;BR /&gt;Is there any difference in the control method or configuration method of TJA1145FD when MCU uses CAN and CAN-FD?&lt;/P&gt;&lt;P&gt;With Best Regards,&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jun 2022 09:34:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-FD-communication-fail-using-TJA1145FD/m-p/1477346#M16012</guid>
      <dc:creator>chengsz12060</dc:creator>
      <dc:date>2022-06-21T09:34:50Z</dc:date>
    </item>
    <item>
      <title>Re: CAN-FD communication fail using  TJA1145FD</title>
      <link>https://community.nxp.com/t5/S32K/CAN-FD-communication-fail-using-TJA1145FD/m-p/1478040#M16029</link>
      <description>&lt;P&gt;Hi&amp;nbsp;chengsz,&lt;/P&gt;
&lt;P&gt;Please check the &lt;STRONG&gt;CFDC&lt;/STRONG&gt; of&amp;nbsp;&lt;EM&gt;CAN control and Transceiver status registers&lt;/EM&gt;. Here is the Data Sheet of &lt;A href="https://www.nxp.com/docs/en/data-sheet/TJA1145.pdf" target="_self"&gt;TJA1145&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="TJA1145 CFDC.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/184213i5BC529BABF6C4925/image-size/large?v=v2&amp;amp;px=999" role="button" title="TJA1145 CFDC.png" alt="TJA1145 CFDC.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;TJA1145 CFDC.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 22 Jun 2022 08:33:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-FD-communication-fail-using-TJA1145FD/m-p/1478040#M16029</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-06-22T08:33:00Z</dc:date>
    </item>
    <item>
      <title>Re: CAN-FD communication fail using  TJA1145FD</title>
      <link>https://community.nxp.com/t5/S32K/CAN-FD-communication-fail-using-TJA1145FD/m-p/1478968#M16047</link>
      <description>&lt;P&gt;I have checked&amp;nbsp;&lt;SPAN&gt;the&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;CFDC&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;of&amp;nbsp; 20h.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;CAN-FD comunication fails if CFDC = 0.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;CAN-FD communcaiton also fails if CFDC = 1.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="20h.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/184404iBB12E31FC97A67A3/image-size/large?v=v2&amp;amp;px=999" role="button" title="20h.png" alt="20h.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;20h.png&lt;/span&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jun 2022 10:06:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-FD-communication-fail-using-TJA1145FD/m-p/1478968#M16047</guid>
      <dc:creator>chengsz12060</dc:creator>
      <dc:date>2022-06-23T10:06:11Z</dc:date>
    </item>
  </channel>
</rss>