<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: CAN VOLTAGE LEVEL</title>
    <link>https://community.nxp.com/t5/S32K/CAN-VOLTAGE-LEVEL/m-p/1476413#M15988</link>
    <description>&lt;P&gt;Hi@asrikrishnagovind&lt;/P&gt;
&lt;P&gt;The test level of the Rx Tx PIN pin of the MCU is about 0~5V.&lt;/P&gt;
&lt;P&gt;br!&lt;/P&gt;</description>
    <pubDate>Mon, 20 Jun 2022 02:57:56 GMT</pubDate>
    <dc:creator>Senlent</dc:creator>
    <dc:date>2022-06-20T02:57:56Z</dc:date>
    <item>
      <title>CAN VOLTAGE LEVEL</title>
      <link>https://community.nxp.com/t5/S32K/CAN-VOLTAGE-LEVEL/m-p/1475974#M15977</link>
      <description>&lt;P&gt;While Powering the S32K144-100LQFP MCU at 5V, what voltage levels are the CAN Tx and Rx operating at? Thanks and Regards&lt;/P&gt;</description>
      <pubDate>Fri, 17 Jun 2022 11:05:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-VOLTAGE-LEVEL/m-p/1475974#M15977</guid>
      <dc:creator>asrikrishnagovind</dc:creator>
      <dc:date>2022-06-17T11:05:22Z</dc:date>
    </item>
    <item>
      <title>Re: CAN VOLTAGE LEVEL</title>
      <link>https://community.nxp.com/t5/S32K/CAN-VOLTAGE-LEVEL/m-p/1476413#M15988</link>
      <description>&lt;P&gt;Hi@asrikrishnagovind&lt;/P&gt;
&lt;P&gt;The test level of the Rx Tx PIN pin of the MCU is about 0~5V.&lt;/P&gt;
&lt;P&gt;br!&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jun 2022 02:57:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-VOLTAGE-LEVEL/m-p/1476413#M15988</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2022-06-20T02:57:56Z</dc:date>
    </item>
  </channel>
</rss>