<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K148 LIN - no communication</title>
    <link>https://community.nxp.com/t5/S32K/S32K148-LIN-no-communication/m-p/1476267#M15982</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Seems to be same problem, as &lt;A href="https://community.nxp.com/t5/S32K/S32K148EVB-Q176-SBC/m-p/1051405#M6950" target="_blank" rel="noopener"&gt;here&lt;/A&gt;&lt;BR /&gt;As my board is also 148, I had to change to LPUART0, as there is only one LIN transceiver. Same goes to chip information&amp;nbsp; etc. and the name of boards, as examples are for 144 board.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;A&lt;/P&gt;</description>
    <pubDate>Sat, 18 Jun 2022 21:24:32 GMT</pubDate>
    <dc:creator>argonaut</dc:creator>
    <dc:date>2022-06-18T21:24:32Z</dc:date>
    <item>
      <title>S32K148 LIN - no communication</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-LIN-no-communication/m-p/1349449#M12296</link>
      <description>&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;I doing some development with an S32K148 devboard with LIN communication. But the problem is that I dont recieve any communication from the LIN port. I have tried both the LIN master and slave example without LIN stack.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I followed the instructions using LIN2 port on the EVB and attached LIN and GND (removed J21 when using Slave). The EVB is connected to an LIN-bus with an external interface to send/receive data to the EVB. But I cannot see any data being sent nor recieved in the EVB. The only time I see data is when I re-plug the power-cable to the EVB.&lt;/P&gt;&lt;P&gt;Am I missing something? Do I need any other cables connected? I have 12V external voltage.&lt;/P&gt;&lt;P&gt;I know that the example is suppose to have 2 EVB, but I only have 1 and a interface which can send data on LIN.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Oct 2021 07:04:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-LIN-no-communication/m-p/1349449#M12296</guid>
      <dc:creator>gregymcwood</dc:creator>
      <dc:date>2021-10-01T07:04:38Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 LIN - no communication</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-LIN-no-communication/m-p/1350630#M12334</link>
      <description>&lt;P&gt;Hello Gregory,&lt;/P&gt;
&lt;P&gt;Which examples exactly have you tried?&lt;/P&gt;
&lt;P&gt;Can you test the lin_master_s32k148 SDK example?&lt;/P&gt;
&lt;P&gt;You should see this signal:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1633439024708.png" style="width: 997px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/158301i2B41D3B74F35F7CF/image-dimensions/997x235?v=v2" width="997" height="235" role="button" title="danielmartynek_0-1633439024708.png" alt="danielmartynek_0-1633439024708.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 05 Oct 2021 13:04:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-LIN-no-communication/m-p/1350630#M12334</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-10-05T13:04:20Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 LIN - no communication</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-LIN-no-communication/m-p/1466961#M15750</link>
      <description>&lt;P&gt;from which pin I should get this?&lt;/P&gt;&lt;P&gt;A&lt;/P&gt;</description>
      <pubDate>Tue, 31 May 2022 18:03:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-LIN-no-communication/m-p/1466961#M15750</guid>
      <dc:creator>argonaut</dc:creator>
      <dc:date>2022-05-31T18:03:16Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 LIN - no communication</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-LIN-no-communication/m-p/1467427#M15760</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201576"&gt;@argonaut&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;In the example mentioned above, it is PTC9.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1654082058149.png" style="width: 730px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/181932iCBAD33D5FFB531C0/image-dimensions/730x418?v=v2" width="730" height="418" role="button" title="danielmartynek_0-1654082058149.png" alt="danielmartynek_0-1654082058149.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 01 Jun 2022 11:14:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-LIN-no-communication/m-p/1467427#M15760</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2022-06-01T11:14:44Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 LIN - no communication</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-LIN-no-communication/m-p/1467501#M15764</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;Can't find PTC9 pin on my board (S32K148EVB-Q176)!&amp;nbsp;I've tried LIN1 and LIN2 pins - no luck.&amp;nbsp;Probably not meant for beginner. No instructions or manuals how to work ok connect etc.&amp;nbsp;Or my board is somehow a mess, cause all i see on picoscope, is just a 12v and no LIN messages.&lt;/P&gt;&lt;P&gt;KR&lt;/P&gt;&lt;P&gt;Argo&lt;/P&gt;</description>
      <pubDate>Wed, 01 Jun 2022 13:36:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-LIN-no-communication/m-p/1467501#M15764</guid>
      <dc:creator>argonaut</dc:creator>
      <dc:date>2022-06-01T13:36:39Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 LIN - no communication</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-LIN-no-communication/m-p/1476267#M15982</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Seems to be same problem, as &lt;A href="https://community.nxp.com/t5/S32K/S32K148EVB-Q176-SBC/m-p/1051405#M6950" target="_blank" rel="noopener"&gt;here&lt;/A&gt;&lt;BR /&gt;As my board is also 148, I had to change to LPUART0, as there is only one LIN transceiver. Same goes to chip information&amp;nbsp; etc. and the name of boards, as examples are for 144 board.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;A&lt;/P&gt;</description>
      <pubDate>Sat, 18 Jun 2022 21:24:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-LIN-no-communication/m-p/1476267#M15982</guid>
      <dc:creator>argonaut</dc:creator>
      <dc:date>2022-06-18T21:24:32Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 LIN - no communication</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-LIN-no-communication/m-p/1596260#M20533</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191941"&gt;@gregymcwood&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I'm facing the same problem, I'm using the s32k148 176pin controller and connecting LIN1 to LIN2 on the same board. but not showing any data. Did you solve your problem? If yes please let me know what kind of changes are required.&lt;/P&gt;</description>
      <pubDate>Thu, 09 Feb 2023 06:39:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-LIN-no-communication/m-p/1596260#M20533</guid>
      <dc:creator>saurabhkulkarni123</dc:creator>
      <dc:date>2023-02-09T06:39:10Z</dc:date>
    </item>
  </channel>
</rss>