<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: UDS client implementation in S32K144EVB</title>
    <link>https://community.nxp.com/t5/S32K/UDS-client-implementation-in-S32K144EVB/m-p/1474906#M15956</link>
    <description>&lt;P&gt;&lt;A href="https://github.com/driftregion/iso14229" target="_blank"&gt;https://github.com/driftregion/iso14229&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 16 Jun 2022 02:09:15 GMT</pubDate>
    <dc:creator>driftregion</dc:creator>
    <dc:date>2022-06-16T02:09:15Z</dc:date>
    <item>
      <title>UDS client implementation in S32K144EVB</title>
      <link>https://community.nxp.com/t5/S32K/UDS-client-implementation-in-S32K144EVB/m-p/1246077#M10183</link>
      <description>&lt;P&gt;Is there any Existing code or example for the implementation of the UDS client in S32K144EVB&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Mar 2021 05:54:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/UDS-client-implementation-in-S32K144EVB/m-p/1246077#M10183</guid>
      <dc:creator>Prkh</dc:creator>
      <dc:date>2021-03-16T05:54:08Z</dc:date>
    </item>
    <item>
      <title>Re: UDS client implementation in S32K144EVB</title>
      <link>https://community.nxp.com/t5/S32K/UDS-client-implementation-in-S32K144EVB/m-p/1246387#M10197</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/184316"&gt;@Prkh&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There is a UDS bootloader:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1615892901484.png" style="width: 737px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/139751i9D31E2780BC13FB4/image-dimensions/737x137?v=v2" width="737" height="137" role="button" title="danielmartynek_0-1615892901484.png" alt="danielmartynek_0-1615892901484.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_0-1615892901484.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/s32k-automotive-mcus/s32k1-microcontrollers-for-general-purpose:S32K1?tab=Design_Tools_Tab" target="_blank" rel="noopener"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/s32k-automotive-mcus/s32k1-microcontrollers-for-general-purpose:S32K1?tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 16 Mar 2021 11:10:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/UDS-client-implementation-in-S32K144EVB/m-p/1246387#M10197</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-03-16T11:10:52Z</dc:date>
    </item>
    <item>
      <title>Re: UDS client implementation in S32K144EVB</title>
      <link>https://community.nxp.com/t5/S32K/UDS-client-implementation-in-S32K144EVB/m-p/1474906#M15956</link>
      <description>&lt;P&gt;&lt;A href="https://github.com/driftregion/iso14229" target="_blank"&gt;https://github.com/driftregion/iso14229&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jun 2022 02:09:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/UDS-client-implementation-in-S32K144EVB/m-p/1474906#M15956</guid>
      <dc:creator>driftregion</dc:creator>
      <dc:date>2022-06-16T02:09:15Z</dc:date>
    </item>
    <item>
      <title>Re: UDS client implementation in S32K144EVB</title>
      <link>https://community.nxp.com/t5/S32K/UDS-client-implementation-in-S32K144EVB/m-p/2297863#M56271</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working on UDS bootloader development for S32K144 using S32 Design Studio 3.4 (RTD/RTM).&lt;/P&gt;&lt;P&gt;In an NXP Community thread, it is mentioned that the Unified Bootloader Framework (UDS over CAN/LIN TP) can be downloaded and used as a reference for UDS bootloader implementation. I have downloaded the Unified Bootloader Framework ZIP, but I need guidance on how to integrate or port it into an S32 Design Studio 3.4 project.&lt;/P&gt;&lt;P&gt;Additionally, I found the following NXP Community ticket where a demo UDS bootloader via CAN is explained:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K144-Bootloader-via-CAN/m-p/1793455" target="_new" rel="noopener"&gt;https://community.nxp.com/t5/S32K/S32K144-Bootloader-via-CAN/m-p/1793455&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Based on this, I would like clarification on whether I should continue using S32 Design Studio 3.4 for bootloader implementation or install S32 Design Studio – ARM version for this purpose.&lt;/P&gt;&lt;P&gt;Could you please clarify the following points:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;Which folders/modules from the Unified Bootloader Framework are mandatory to port for a basic UDS bootloader (for example, UDS services, TP layer, CAN abstraction)?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is the Unified Bootloader Framework intended to be used only as a standalone reference, or can it be directly integrated into an existing S32DS RTD-based bootloader project?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is this framework still recommended for new designs, or is there a newer UDS/bootloader solution available for S32K devices?&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Any guidance or a recommended folder structure for porting would be very helpful.&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jan 2026 05:52:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/UDS-client-implementation-in-S32K144EVB/m-p/2297863#M56271</guid>
      <dc:creator>KAVIN7</dc:creator>
      <dc:date>2026-01-22T05:52:47Z</dc:date>
    </item>
  </channel>
</rss>