<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FXLS90322 I2C Function in S32K</title>
    <link>https://community.nxp.com/t5/S32K/FXLS90322-I2C-Function/m-p/1471875#M15875</link>
    <description>&lt;P&gt;Hi :&lt;/P&gt;&lt;P&gt;I use S32K144 as MCU ，and the SDK Vision&amp;nbsp; is 4.0.2.&lt;/P&gt;&lt;P&gt;i Are there any Setting i must make before using the I2C communication Function of the FXLS90322?&lt;/P&gt;&lt;P&gt;I cannot receive the ACK bit from the slave while writing the address(the address had already&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;moved over by 1 bit&lt;/SPAN&gt;)&lt;/P&gt;&lt;P&gt;From the time sequence captured by oscilloscope, the time sequence of I2C is also normal, but still can not receive the ACK bit sent from the FXLS90322.&lt;/P&gt;&lt;P&gt;BTW,when I used FlexIO to simulate I2C communication, the error status I received was I2C_RX_Overrun&lt;/P&gt;&lt;P&gt;Looking forward for your reply.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/12216" target="_blank"&gt;@TomasVaverka&lt;/A&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 10 Jun 2022 01:28:29 GMT</pubDate>
    <dc:creator>Lin_SiuU</dc:creator>
    <dc:date>2022-06-10T01:28:29Z</dc:date>
    <item>
      <title>FXLS90322 I2C Function</title>
      <link>https://community.nxp.com/t5/S32K/FXLS90322-I2C-Function/m-p/1471875#M15875</link>
      <description>&lt;P&gt;Hi :&lt;/P&gt;&lt;P&gt;I use S32K144 as MCU ，and the SDK Vision&amp;nbsp; is 4.0.2.&lt;/P&gt;&lt;P&gt;i Are there any Setting i must make before using the I2C communication Function of the FXLS90322?&lt;/P&gt;&lt;P&gt;I cannot receive the ACK bit from the slave while writing the address(the address had already&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;moved over by 1 bit&lt;/SPAN&gt;)&lt;/P&gt;&lt;P&gt;From the time sequence captured by oscilloscope, the time sequence of I2C is also normal, but still can not receive the ACK bit sent from the FXLS90322.&lt;/P&gt;&lt;P&gt;BTW,when I used FlexIO to simulate I2C communication, the error status I received was I2C_RX_Overrun&lt;/P&gt;&lt;P&gt;Looking forward for your reply.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/12216" target="_blank"&gt;@TomasVaverka&lt;/A&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 10 Jun 2022 01:28:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FXLS90322-I2C-Function/m-p/1471875#M15875</guid>
      <dc:creator>Lin_SiuU</dc:creator>
      <dc:date>2022-06-10T01:28:29Z</dc:date>
    </item>
  </channel>
</rss>